Other Parts Discussed in Thread: TMS570LS3137, HALCOGEN
Hi,
Can I use printf function for writing in console in Tms570ls3137 ? Addionality, I use FreeRtos, and compiler is Code Composer
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS570LS3137, HALCOGEN
Hi,
Can I use printf function for writing in console in Tms570ls3137 ? Addionality, I use FreeRtos, and compiler is Code Composer
Hans,
Yes, but the printf function that comes with the TI ARM C compiler uses breakpoints to implement console IO, and the console IO is scanned over JTAG. So a) it will be time-intrusive and b) it won't give you something you can connect to over a serial port, without Code Composer.
If you're debugging, and using the printf non-realtime say to print out cycle counts before & after some algorithm that you are benchmarking then this is probably fine.
If you need printf() over a UART say to run without CCS attached and without halting the processor, then the C Compiler manual explains how to map the low level IO to another device like a UART.
I'm not aware of any canned example of this though that we can send you. One of my colleagues has done something close though so I'll add him to this thread.
Thank you for reply. but I do not want to more complex thing. I used puts(); function, but I took Dabort exception.. But I use sprintf and it works but too slow..Why is when ı use puts, take dabort fault.
Hans,
Here is a simple CCS project that I've created to redirect the printf to a serial terminal.
The project includes Halcogen configuration files.
It uses the SCI2 that is connect to the USB port of our HDK.
The serial communication has to be set as:
115200 bits per second
8 Bits data
1 Stop (No parity)
In the project properties, the following symbol has to be defined: UART_SUPPORT otherwise the regular printf will be used.
Please have a try and let me know if this is useful.