Other Parts Discussed in Thread: EK-TM4C123GXL
I need to transmit 40 bits width maintaining Fss and Clock active during the transmission of 40 bits of data in mode 0
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: EK-TM4C123GXL
I need to transmit 40 bits width maintaining Fss and Clock active during the transmission of 40 bits of data in mode 0
Hi,
Should I understand you don' t know where/how to start up with this problem of 40 bits? If yes, then maybe you provide more info - what is the device to drive - usually in cases like this a configuration of five words of 8 bits each would be a good solution. Place them one after another into FIFO and then wait until FIFO is empty. Take into account the mode 0 requested by you in the first post would not give you Fss low for the duration of all these 40 bits. Mode 0 works only with Fss rising up after each word, so you must choose another mode ( that's why I asked you what is the device) .
Petrei
Hi,
You can use SPO=0 and SPH=1 with DSS=8. But you have to make sure that the FIFO is written with the 5 bytes so that they can transmitted in continous mode and the CS remain low for the 40 bits.
Regards
Amit