Hi,all
I use the code in "NoRTOS_CCS_RM46" project ,and I find something inconvenient.After I programming the TMS570LS3137 ,then turn on power, the program dosn't run ,I use CCS V5.2 connecting TMS570LS3137,and the program stop at asm(“ b #-8”) ,then I add 4 to PC register, then the program run .
The problem is in normal use , no one can do the operation described above.How to use TPS65381 easily?
Hope to get answer soon. Thanks a lot.