Dear Members,
The example: enet_lwip contains the following line:
lwIPInit (g_ui32SysClock, pui8MACArray, 0, 0 ,0, IPADDR_USE_DHCP);
With this line, the evaluation board gets an IP address from DHCP server.
I changed it to:
lwIPInit (g_ui32SysClock, pui8MACArray, inet_addr ("3.1.168.192"), inet_addr ("0.0.255.255"),0, IPADDR_USE_STATIC);
But it seems the TIVA does not get the proper IP address: 192.168.1.3
I opened an Internet browser with this address and got nothing.
I also tried the line:
lwIPInit (g_ui32SysClock, pui8MACArray, 0xC0A80103, 0xFFFF0000,0, IPADDR_USE_STATIC);
and got the same problem.
There is a line:
Ui32NewIpAddress = lwIPLocalIPAddrGet ();
The value if Ui32NewIpAddress is not the new IP.
Can you help ?
Thanks,
Zvika