hi, as the title says, i'm using tm4c123g with TMP136GZ temerature sensor. Now i have a wrong conversion, about double of the real temperature. I followed this topic to configure tivac:
http://e2e.ti.com/support/microcontrollers/tiva_arm/f/908/t/296196.aspx
but it's the same, i obtain a value of 50 celsius degrees.
now i tried with stellaris launchpad and it's ok
here is the cde for the adc:
void tmp36gz_setup(){
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
ADCReferenceSet(ADC0_BASE, ADC_REF_INT);
GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_5);
ADCSequenceDisable(ADC0_BASE, 3);
ADCSequenceConfigure(ADC0_BASE, 3, ADC_TRIGGER_PROCESSOR, 0);
ADCSequenceStepConfigure(ADC0_BASE, 3, 0, ADC_CTL_CH8| ADC_CTL_IE |ADC_CTL_END);
ADCSequenceEnable(ADC0_BASE, 3);
ADCIntClear(ADC0_BASE, 3);
}
void tmp36gz_acquisisci(uint32_t *dato){
ADCProcessorTrigger(ADC0_BASE, 3);
while (!ADCIntStatus(ADC0_BASE, 3, false));
ADCSequenceDataGet(ADC0_BASE, 3, dato);
ADCIntClear(ADC0_BASE, 3);
}