Other Parts Discussed in Thread: TM4C1294NCPDT, TM4C129ENCPDT
Hello,
In the TM4C1294NCPDT data sheet, version December 12, 2013, at the bottom of Table 27-15 there's a footnote which states "The capacitor should be connected as close as possible to pin ." (sic) I'm using the recommended combination of 2.2uF, 1.0uF, 100nF, and 10nF capacitors. Which pin, 87 or 115 should get the larger capacitor value?
BTW, the System Design Guideline document is excellent.
I looked at the data sheet for the TM4C129ENCPDT but it also has the same omission.
Thanks,
Derek