Other Parts Discussed in Thread: LMFLASHPROGRAMMER, UNIFLASH
I have developed my first prototype using the Tiva C LaunchPad and CC3000 Booster Pack, and most things are working as desired.
I now have a custom board being developed that uses the exact same Tiva C MCU that comes with the Tiva C LaunchPad. The board is based on the reference designs that come with the Tiva C LaunchPad and the CC3000.
What changes if any will be required with my code?
I am using TI-RTOS and CCS, will I need to edit board files or any other configurations or code. Or do I need to do nothing except select the programmer/emulator (XDS200) in the CCS settings for my project?
Yes...this is the first time I have had a custom board developed from dev boards, so this is all new to me.
Glenn.