I have found useful posts on how to use SysCtlDelay to implement a usec delay function. (all my controllers run at > 1MHz). So I ended up with a function that reads like:
inline void TMR_DelayUS(UINT8 usec) {
// See user TivaWare user guide or
// http://e2e.ti.com/support/microcontrollers/stellaris_arm/f/471/t/143842.aspx
// or search for SysCtlDelay
SysCtlDelay(usec*SysCtlClockGet()/1000000/3);
}
If I were to write this function my self using a timer, I would have to consider timer overflow. I assume SysCtlDelay is using the sys clock timer, but does the code consider when the timer overflows?
Warning: I have still not written a GPIO toggle function and put the above code to a test with an oscilliscope.
P.S. see below for better code.