Other Parts Discussed in Thread: TMS570LS2124
Hi,
TMS570LS2124
I am reading a shared input pin in both ADC1 and ADC2, in this example AD1IN[16]/AD2IN[0]. Both are within the same event group, each of which is triggered from the same HET channel. Both ADC modules and event groups are configured the same way, they have the same sample time and same discharge time and are sampling the same number of input channels. The input voltage of the channel sampled immediately prior to AD1IN[16]/AD2IN[0] is at 0V.
I would expect each ADC reading to be the same (within 1 bit error). Same input voltage measured at exactly the same time on ADC modules configured in exactly the same way.
I am however, seeing a 5 or 6 bit difference between the two readings (see attached trace).
Can anybody explain why this is so?
Regards, Tony.