Other Parts Discussed in Thread: HALCOGEN
Dear friends,
I use Sci2 (LIN) RX and TX dma in my code, DMA BTC irq is enabled and this irq calls:
void dmaGroupANotification(dmaInterrupt_t inttype, sint32 channel)
{
if(channel == DMA_CH9)
{
DMA_TX_Flag = 0x5555BBBB;
scilinREG->CLEARINT |= SCI_TX_DMA;
}
else if(channel == DMA_CH10)
{
DMA_RX_Flag = 0x5555AAAA;
}
}
function, where SCI_TX_DMA = (1 << 16),
I expect to disable only TX_DMA, but, writing any value to scilinREG->CLEARINT register causes this register to change its value to 0, so my RX_DMA goes disabled mode.
How can I successfully write to this register. Register definition is:
#define scilinREG ((sciBASE_t *)0xFFF7E400U)
sciBASE_t is:
typedef volatile struct sciBase
{
uint32 GCR0; /**< 0x0000 Global Control Register 0 */
uint32 GCR1; /**< 0x0004 Global Control Register 1 */
uint32 rsdv1; /**< 0x0008 Global Control Register 2 */
uint32 SETINT; /**< 0x000C Set Interrupt Enable Register */
uint32 CLEARINT; /**< 0x0010 Clear Interrupt Enable Register */
uint32 SETINTLVL; /**< 0x0014 Set Interrupt Level Register */
uint32 CLEARINTLVL; /**< 0x0018 Set Interrupt Level Register */
uint32 FLR; /**< 0x001C Interrupt Flag Register */
uint32 INTVECT0; /**< 0x0020 Interrupt Vector Offset 0 */
uint32 INTVECT1; /**< 0x0024 Interrupt Vector Offset 1 */
uint32 FORMAT; /**< 0x0028 Format Control Register */
uint32 BRS; /**< 0x002C Baud Rate Selection Register */
uint32 ED; /**< 0x0030 Emulation Register */
union //TODO: DMA for RX için bunu RD yerine ekle, sci.c içinde gereken değişiklikleri yap
{
unsigned int RD;
struct
{
unsigned int : 24;
unsigned char RD_UC;
}SCIRD_ST;
}SCIRD_UN;
//uint32 RD; /**< 0x0034 Receive Data Buffer */
union /* 0x38 */
{
unsigned int TD;
struct
{
unsigned int : 24;
unsigned char TD_UC; /*0x3B*/ //Big endian uC: TMS570
}SCITD_ST;
}SCITD_UN;
//uint32 TD; /**< 0x0038 Transmit Data Buffer */
uint32 PIO0; /**< 0x003C Pin Function Register */
uint32 PIO1; /**< 0x0040 Pin Direction Register */
uint32 PIO2; /**< 0x0044 Pin Data In Register */
uint32 PIO3; /**< 0x0048 Pin Data Out Register */
uint32 PIO4; /**< 0x004C Pin Data Set Register */
uint32 PIO5; /**< 0x0050 Pin Data Clr Register */
uint32 PIO6; /**< 0x0054: Pin Open Drain Output Enable Register */
uint32 PIO7; /**< 0x0058: Pin Pullup/Pulldown Disable Register */
uint32 PIO8; /**< 0x005C: Pin Pullup/Pulldown Selection Register */
uint32 rsdv2[12U]; /**< 0x0060: Reserved */
uint32 IODFTCTRL; /**< 0x0090: I/O Error Enable Register */
} sciBASE_t;
which is in the Halcogen generated file: reg_sci.h
I know it is a volatile struct, so tried to modify it into irq subroutine, but it is also unsuccessfull.
So, what I need is, just to disable TX_DMA, but not touch RX_DMA
I do not prefer disabling TX pin by TXENA, SCILIN->CLEARINT is best solution if it works.
thanks in advance
regards
Levent