Other Parts Discussed in Thread: TM4C123GH6PM
I am using the TIVA C (TM4C123GH6PM) launchpad, and I am trying to create 2 digital signals. I need a 500kHz output with a 50% duty cycle, and a 25kHz output with a 20% duty cycle. These signals need to be low jitter and synchronized so that the falling edge happens at the same time for both signals. Here is what I have so far using the PWM modules, but I am unable to get the falling edges to line up. I don't want the timing of these to be affected by other things going on in the processor, so that's why I picked PWMs.
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_gpio.h"
#include "inc/hw_types.h"
#include "inc/hw_memmap.h"
#include "driverlib/sysctl.h"
#include "driverlib/pin_map.h"
#include "driverlib/gpio.h"
#include "driverlib/pwm.h"
#define GPIO_PB6_M0PWM0 0x00011804
#define GPIO_PB7_M0PWM1 0x00011C04
#define GPIO_PB4_M0PWM2 0x00011004
#define GPIO_PB5_M0PWM3 0x00011404
#define GPIO_PE4_M0PWM4 0x00041004
#define GPIO_PE5_M0PWM5 0x00041404
#define GPIO_PF1_M1PWM5 0x00050405
#define GPIO_PF2_M1PWM6 0x00050805
#define GPIO_PF3_M1PWM7 0x00050C05
int
main(void)
{
//Set the clock
SysCtlClockSet(SYSCTL_SYSDIV_2_5|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_INT); // SET SYSTEM CLOCK FOR 80Mhz, off of PLL
//Configure PWM Clock to match system
SysCtlPWMClockSet(SYSCTL_PWMDIV_1);
// Enable the peripherals used by this program.
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM1); //The Tiva Launchpad has two modules (0 and 1). Module 1 covers the LED pins
//Configure PF1,PF2,PF3 Pins as PWM
GPIOPinConfigure(GPIO_PF1_M1PWM5);
GPIOPinConfigure(GPIO_PF2_M1PWM6);
GPIOPinTypePWM(GPIO_PORTF_BASE, GPIO_PIN_1 | GPIO_PIN_2);
//Configure PWM Options
PWMGenConfigure(PWM1_BASE, PWM_GEN_2, PWM_GEN_MODE_UP_DOWN | PWM_GEN_MODE_NO_SYNC);
PWMGenConfigure(PWM1_BASE, PWM_GEN_3, PWM_GEN_MODE_UP_DOWN | PWM_GEN_MODE_NO_SYNC);
//Set the Period (expressed in clock ticks)
PWMGenPeriodSet(PWM1_BASE, PWM_GEN_2, 160);
PWMGenPeriodSet(PWM1_BASE, PWM_GEN_3, 3200);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_5,80); //set 50% duty cycle
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_6,2560); //set 20% duty cycle
// Enable the PWM generator
PWMGenEnable(PWM1_BASE, PWM_GEN_2);
PWMGenEnable(PWM1_BASE, PWM_GEN_3);
// Turn on the Output pins
PWMOutputState(PWM1_BASE, PWM_OUT_5_BIT | PWM_OUT_6_BIT, true);
//Do nothing (will handle other tasks later on)
while(1);
}
Right now, the 25kHz falling edge happens .5us after the falling edge of the 500kHz. Are there any suggestions on how to fix this?
Thanks.