This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Some TivaWare 2.0.1.11577 CCS projects still refer to Stellaris rather than Tiva devices

In TivaWare 2.0.1.11577 the CCS projects for the examples have the device type set to Tiva devices. However, the driverlib, grlib and usblib CCS projects still have the device type set to Stellaris devices.

 This means that to compile the example, driverlib, grlib and usblib CCS projects during the CCS installation processor support for both "Stellaris Cortex M MCUs" as well as "Tiva C Series ARM MCUs" must be selected. Failure to do so can cause "This project was created for a device that is not currently recognized: Cortex M.LM4F110B2QR." errors to be reported when attempting to compile the  driverlib, grlib and usblib CCS projects. This can cause frustration for new users attempting to follow the tutorial in http://www.ti.com/lit/ml/spmu352/spmu352.pdf - e.g. see #10010 and #10056 erorrs in ALL example programs.

Can the projects in TivaWare be updated to consistently only refer to Tiva devices?