Other Parts Discussed in Thread: RM42L432, HALCOGEN
Hi,
I want to use the RM42L432 Launchpad for obtaining a Timestamp with high resolution (HR bits should show meaningful data) at pins 0, 2 and 4 simultaneously.
The code I wrote in the HET IDE looks like this:
L00 CNT {reg=A, max=1ffffffh}
L01 WCAP {next=L02, cond_addr=L02, hr_lr=high, reg=A, event=RISE, pin=0, data=0}
L02 WCAP {next=L03, cond_addr=L03, hr_lr=high, reg=B, event=RISE, pin=2, data=0}
L03 WCAP {next=L04, cond_addr=L04, hr_lr=high, reg=T, event=RISE, pin=4, data=0}
L04 BR {next=L00, cond_addr=L00, event=NOCOND};
I have assembled it and I have a .h and a .c file for the above code.
I entered their locations in the NHET driver settings of Halcogen.
How do I integrate this code with my main code using CCS? (The main code does operations on these timestamp values.)
Regards,
Nimit.