Other Parts Discussed in Thread: TM4C123GH6PM
Hi all,
I am writing a code to interface TM4C123GH6PM with RTC (PCF8563) over I2C. I have written a sample code for testing, to write to RTC registers and read back from them. When i execute the code it gets stuck in while loop (while(I2CMasterBusy(I2C0_BASE))) forever. I am using Tiva C series launch pad board and CCS 5.5.0 for development. Any help or suggestion would be appreciated.
I have one more querry, do we really need to use this ( GPIOPinTypeI2CSCL(GPIO_PORTB_BASE, GPIO_PIN_2);) line in the code.
Code is below :
#define NUM_I2C_DATA 8
#define SLAVE_ADDRESS 0x51
#define SLAVE_ADDRESS 0x51
#define TIME_REGISTER_START_ADDR 0x02
#define SECONDS 0x01
#define MINUTES 0x50
#define HOURS 0x21
#define DAYS 0x21
#define WEEKDAYS 0x02
#define C_MONTHS 0x01
#define YEARS 0x14
int main()
{
uint32_t pui32DataTx[NUM_I2C_DATA];
uint32_t pui32DataRx[NUM_I2C_DATA];
uint32_t ui32Index;
//
// Initialize the receive buffer to NULL.
//
for(ui32Index = 0; ui32Index < NUM_I2C_DATA; ui32Index++)
{
pui32DataRx[ui32Index] = 0;
}
// Write TIME Registers data into RTC
//
// Set the clocking to run directly from the external crystal/oscillator.
// TODO: The SYSCTL_XTAL_ value must be changed to match the value of the
// crystal on your board.
//
SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);
//
// The I2C0 peripheral must be enabled before use.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);
//
// For this example I2C0 is used with PortB[3:2]. The actual port and
// pins used may be different on your part, consult the data sheet for
// more information. GPIO port B needs to be enabled so these pins can
// be used.
// TODO: change this to whichever GPIO port you are using.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
//
// Configure the pin muxing for I2C0 functions on port B2 and B3.
// This step is not necessary if your part does not support pin muxing.
// TODO: change this to select the port/pin you are using.
//
GPIOPinConfigure(GPIO_PB2_I2C0SCL);
GPIOPinConfigure(GPIO_PB3_I2C0SDA);
//I2CMasterEnable(GPIO_PORTB_BASE);
GPIOPinTypeI2CSCL(GPIO_PORTB_BASE, GPIO_PIN_2);
//
// Select the I2C function for these pins. This function will also
// configure the GPIO pins pins for I2C operation, setting them to
// open-drain operation with weak pull-ups. Consult the data sheet
// to see which functions are allocated per pin.
// TODO: change this to select the port/pin you are using.
//
GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_2 | GPIO_PIN_3);
//
// Enable and initialize the I2C0 master module. Use the system clock for
// the I2C0 module. The last parameter sets the I2C data transfer rate.
// If false the data rate is set to 100kbps and if true the data rate will
// be set to 400kbps. For this example we will use a data rate of 100kbps.
//
I2CMasterInitExpClk(I2C0_BASE, SysCtlClockGet(), false);
//
// Tell the master module what address it will place on the bus when
// communicating with the slave. Set the address to SLAVE_ADDRESS
// (as set in the slave module). The receive parameter is set to false
// which indicates the I2C Master is initiating a writes to the slave. If
// true, that would indicate that the I2C Master is initiating reads from
// the slave.
//
//I2CMasterSlaveAddrSet(I2C0_BASE, SLAVE_ADDRESS, false);
I2CMasterSlaveAddrSet(I2C0_BASE, SLAVE_ADDRESS, false);
//
// Initalize the data to send.
//
pui32DataTx[0] = TIME_REGISTER_START_ADDR;
pui32DataTx[1] = SECONDS;
pui32DataTx[2] = MINUTES;
pui32DataTx[3] = HOURS;
pui32DataTx[4] = DAYS;
pui32DataTx[5] = WEEKDAYS;
pui32DataTx[5] = C_MONTHS;
pui32DataTx[6] = YEARS;
#if 1
//
// Send pieces of I2C data from the master to the slave.
//
for(ui32Index = 0; ui32Index < NUM_I2C_DATA; ui32Index++)
{
//
// Place the data to be sent in the data register
//
I2CMasterDataPut(I2C0_BASE, pui32DataTx[ui32Index]);
//
// Initiate send of data from the master. Since the loopback
// mode is enabled, the master and slave units are connected
// allowing us to receive the same data that we sent out.
//
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_SINGLE_SEND);
//
// Wait until master module is done transferring.
//
while(I2CMasterBusy(I2C0_BASE))
{
}
}
#endif
//
// Read TIME Registers data from RTC
//
//
// Modifiy the data direction to true, so that seeing the address will
// indicate that the I2C Master is initiating a read from the slave.
//
I2CMasterSlaveAddrSet(I2C0_BASE, SLAVE_ADDRESS, true);
for(ui32Index = 0; ui32Index < NUM_I2C_DATA; ui32Index++)
{
//
// Tell the master to read data.
//
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_SINGLE_RECEIVE);
//
// Read the data from the master.
//
pui32DataRx[ui32Index] = I2CMasterDataGet(I2C0_BASE);
}
return (0);
}
Thanks & Regards