Other Parts Discussed in Thread: TM4C123GH6PM
Hai friend
I am tring eeprom interface with tiva TM4C123GH6PM in ccs ide . I have problem in reading and writing please any one help me .
this is my code,
void i2cinit(void)
{
SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
GPIOPinConfigure(GPIO_PB2_I2C0SCL);
GPIOPinConfigure(GPIO_PB3_I2C0SDA);
// Give control to the I2C0 Module
//GPIODirModeSet(GPIO_PORTB_BASE, GPIO_PIN_3, GPIO_DIR_MODE_HW);
//GPIODirModeSet(GPIO_PORTB_BASE, GPIO_PIN_2, GPIO_DIR_MODE_HW);
GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_2 | GPIO_PIN_3);
HWREG(I2C0_BASE + I2C_O_MCR) |= 0x01;
I2CMasterInitExpClk(I2C0_BASE, SysCtlClockGet(), false);
//I2CSlaveEnable(I2C0_BASE);
//I2CSlaveInit(I2C0_BASE, SLAVE_ADDRESS);
I2CMasterEnable(I2C0_BASE);
}
void eepromWrite(uint16_t address_u16, uint8_t data_u8)
{
I2CMasterSlaveAddrSet(I2C0_BASE, SLAVE_ADDRESS, false);
I2CMasterDataPut(I2C0_BASE, ((address_u16 >> 8) & 0xFF));
SysCtlDelay(dalay);
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_START);
while(I2CMasterBusy(I2C0_BASE)) {}
I2CMasterDataPut(I2C0_BASE, (address_u16 & 0xFF));
SysCtlDelay(dalay);
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_START);
while(I2CMasterBusy(I2C0_BASE)) {}
I2CMasterDataPut(I2C0_BASE, data_u8);
SysCtlDelay(dalay);
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_START);
while(I2CMasterBusy(I2C0_BASE)) {}
}
void eepromRead(uint16_t address_u16, uint8_t *rxdata_pu8,uint32_t rxdataLen_u32)
{
uint16_t i = 0;
I2CMasterSlaveAddrSet(I2C0_BASE, SLAVE_ADDRESS, false);
I2CMasterDataPut(I2C0_BASE, ((address_u16 >> 8) & 0xFF));
SysCtlDelay(dalay);
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_START);
while(I2CMasterBusy(I2C0_BASE)) {}
I2CMasterDataPut(I2C0_BASE, (address_u16 & 0xFF));
SysCtlDelay(dalay);
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_START);
while(I2CMasterBusy(I2C0_BASE)) {}
I2CMasterSlaveAddrSet(I2C0_BASE, SLAVE_ADDRESS, true);
while(I2CMasterBusy(I2C0_BASE)) {}
// Tell the master to read data.
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_SINGLE_RECEIVE);
// Wait until the slave is done sending data.
for(i = 0; i < rxdataLen_u32; i++)
{
while(I2CMasterBusy(I2C0_BASE)) {}
*rxdata_pu8 = I2CMasterDataGet(I2C0_BASE);
rxdata_pu8++;
SysCtlDelay(dalay);
}
}