This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Basic problem with two timers

Other Parts Discussed in Thread: EK-TM4C123GXL

I am just about to start using timers for my project and I got stuck immediately with the startup sequence. Timer0 is used to check for incoming data over a TCP link, timer1 is going to be used to control the timing of a AFE.
If anyone can point me directly to the first few places on ti.com or know some code examples that I should look at I would be very grateful! I am using the Tiva C EK-TM4C123GXL with the CC3000.
In the ccs.c filer:
// External declarations for the interrupt handlers used by the application.
extern void Timer0IntHandler( void );
extern void Timer1IntHandler( void );
 
void (* const g_pfnVectors[])( void) = {( void (*)( void ))((unsigned long)&__STACK_TOP),
Timer0IntHandler,                       // Timer 0 subtimer A
Timer1IntHandler,                       // Timer 1 subtimer A
The code I am using in my main.c:
void HWinit( void )
{
        FPULazyStackingEnable ();   //Allows floating-point instructions.
        SysTickPeriodSet (SysCtlClockGet () / SYSTICK_PER_SEC); //
        SysTickIntEnable ();//
        SysTickEnable ();//
 
        // Initializes the CPU usage measurement module with the usage of timer 2.
        CPUUsageInit (SysCtlClockGet (), SYSTICK_PER_SEC, 2); //
 
        // MCU set @ 50Mhz, NOT stable @ 80Mhz!
       SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
 
        //-------------- Enable peripherals ---------------------------------------------------------
        SysCtlPeripheralClockGating (true);                // Enable peripherals to operate when CPU is in sleep
        SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);       // Enable SSI0 peripheral AFE
        SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI1);       // Enable SSI1 peripheral uDMA
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);      // Enables port PA2 and PA4 for SSI0
        SysCtlPeripheralEnable (SYSCTL_PERIPH_GPIOC);     // 
        SysCtlPeripheralEnable (SYSCTL_PERIPH_GPIOD);     // 
        SysCtlPeripheralEnable (SYSCTL_PERIPH_GPIOF);     // 
 
        SysCtlPeripheralEnable (SYSCTL_PERIPH_UART0);     // Virtual port
 
        SysCtlPeripheralEnable (SYSCTL_PERIPH_TIMER0);    // Acquisition frequency
 
        //-------------- Enable peripherals Sleep Mode ----------------------------------------------------
        SysCtlPeripheralSleepEnable (SYSCTL_PERIPH_SSI0);        // Enable SSI0 peripheral Sleep for AFE
 
        GPIOPinTypeGPIOOutput (GPIO_PORTF_BASE, GPIO_PIN_2); //Enable pin for LED PF2
 
        //-------------- AFE SPI (SSI0) -------------------------------------------------------------------
 
        GPIOPinConfigure (GPIO_PA2_SSI0CLK);
        GPIOPinConfigure (GPIO_PA4_SSI0RX);
 
        // Configure the GPIO settings for the SSI pins.  This function also gives control of these pins to the SSI hardware.
        GPIOPinTypeSSI (GPIO_PORTA_BASE, GPIO_PIN_4 | GPIO_PIN_2);
 
        // Configure and enable the SSI port for SPI master mode.
        SSIConfigSetExpClk (SSI0_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0, SSI_MODE_MASTER, 1000000, 16);
 
        // Enable SSI0 interrupt
        IntEnable (INT_SSI0);
 
        // SSI0 is configured to use uDMA
        SSIDMAEnable (SSI0_BASE, SSI_DMA_TX | SSI_DMA_RX);
 
        // Enable the SSI0 module.
        SSIEnable (SSI0_BASE);
 
        unsigned long ulDataRx;
        while (SSIDataGetNonBlocking (SSI0_BASE, &ulDataRx))
       {
       }
 
 
        // -------------- INIT TIMERS -------------------------------------------------------------------
 
        // Enable processor interrupts.
        IntMasterEnable ();
 
        // Configure 32-bit periodic timers.
        TimerConfigure (TIMER0_BASE, TIMER_CFG_PERIODIC);
        TimerConfigure (TIMER1_BASE, TIMER_CFG_PERIODIC); The system crashes here!
 
        TimerLoadSet (TIMER0_BASE, TIMER_A, SysCtlClockGet());
        TimerLoadSet (TIMER1_BASE, TIMER_A, SysCtlClockGet ());
 
        // Setup the interrupts for the timer timeouts.
        IntEnable (INT_TIMER0A);
        IntEnable (INT_TIMER1A);
 
        TimerIntEnable (TIMER0_BASE, TIMER_TIMA_TIMEOUT);
        TimerIntEnable (TIMER1_BASE, TIMER_TIMA_TIMEOUT);
}
When the system crashes it ends up in:
static void
FaultISR( void )
{
    //
    // Enter an infinite loop.
    //
    while (1)
    {
    }
}
 
And I can not see what I have done wrong in the startup sequence.