Other Parts Discussed in Thread: TM4C123GH6PM, UNIFLASH
I have been working through the TM4C123G Launchpad workshop workbook and can't seem to get the CCS new CCS project wizard to include the necessary startup/vector table code. (CCS Version: 5.4.0.00091)
The file specified in the workbook (tm4c123gh6pm_startup_ccs.c) only seems to exist in the uniflash installation, which is where I eventually managed to manually copy it from. The uniflash installation seems to have setup files for most other device derivatives too.
Now, I have been able to find what I assume is a generic startup_ccs.c file in the Tivaware examples tree, and one occurrence in the CCs tree, but it is not added by the CCS project wizard as indicated in the workbook.
Have things changed or did I do something wrong? (I notice that some of the labels in the workbook screenshots are different to what I get listed in my CCS installation but no idea if these are critical or not)
Can the generic "startup_ccs" be used for all device derivatives?
As expected using the tm4c123gh6pm_startup_ccs.c file seems to work correctly on the launchpad but I have not tried the generic version yet. (It looks the same, but there might be some subtle difference I missed).
BR,
Steve