HI when trying to use XDS200 and TM4C129X development board. I get the following message:
Error connecting to the target:
(Error -1265 @ 0x0)
Device ID is not recognized or is not supported by driver. Confirm device and emulator configuration is correct, or update device driver.
(Emulation package 5.1.232.0)
XDS200 is connected to J3 using the 20 pin adapter supplied by Spectrum Digital.
I configured project settings to use Texas Instruments XDS2xx USB emulator. Everything doesworks with the ICDI USB but not the XDS200 with same code etc.
Any idea what how to resolve this?
Thanks
Glenn