Other Parts Discussed in Thread: NOWECC, RM48L950
I am trying to set up SECDED on an RM48L950. The nowECC memory map parameter has 5 options: -F021 16M_ADD, -F021 16M_NOADD, -F021 8M, -F035, -LF035, -F05. It's not clear which of these match the RM48, which has 3M of flash. I have generated output files using the 3 "-F021" options and loaded them at the addresses specified in the nowFlash User's Guide and each time I generate an abort inside of checkFlashECC(). I am using IAR Embedded Workshop, Functional Safety Edition 6.5. Is there a set of nowECC command line parameters that work with the RM48L950 that work in this case?
Thanks,
Bobby Goldberg