Other Parts Discussed in Thread: HALCOGEN
Hi,
I'm working with RM48HDK.I'm using the RTI to trigger ADC in single mode. The tTotal shown by halcogen is not in agreement with the time between trigger (if I set the higher tTime which should be compatible with the time between the trigger the ADC loses a lot of data)
Using the documented formula 13*cycleTime + tSample (as shown by Halcogen as tTotal) does not work with high trigger frequency (~1MHz).
I need to optimize the sample time to maximize signal to noise ratio. How can I calculate the total time required for a single ADC?
Thank you