Other Parts Discussed in Thread: EK-TM4C1294XL, EK-TM4C123GXL
Hi,
Whenever I connect power supply to the launchpad, the controller starts getting heated slowly. Resistance between VDD and GND is low. But I can dump the code using CCS. I have tested 'BLINKY' project. It works.
To my surprise, 400mA voltage regulator on the board doesn't get heated at all. How can this be possible? After all controller gets current from voltage regulator. If the controller has an internal short, it should draw huge current from the regulator and the regulator must be heating up along with the controller.
Can someone explain this strange behavior. Is there anything that i can do to stop the controller getting heated.
Thanks in advance