Other Parts Discussed in Thread: HALCOGEN, TMS570LS0432
Hi guys,
I am looking into Flash Eeprom Emulation (FEE) using the TI FEE library generated by HALCoGen. However there are no option to generate FEE code if I want to create an RM42L43 project.
However that option is available if I select the TMS570LS0432 processor, which has the same memory map as far as I can tell from the datasheet.
Will the code generated for TMS570LS0432 be compatible with my RM42L43 MCU or can I do something else to make HALCoGen support my processor ? :)
I am using HALCoGen 3.06.00
Kind regards
Mikkel