Other Parts Discussed in Thread: LM393
Hi Guys,
I'm using the FreeRTOS demo that came with the Stellaris files and want to add a quadrature encoder interface.
Although CCS doesn't give me an error, the µc freezes when I want to configure the interface?
Also I needed to add the register settings manually to the pin_map.h
in pin_map.h I've added:
// LM4F120H5QR Port/Pin Mapping Definitions
#define GPIO_PC5_PHA1 0x00021406
#define GPIO_PC6_PHB1 0x00021806
Here's my code, like I said when adding the QEI configuration (code in bold) the µc freezes but I don't get an error.
When I comment the code out, everything works fine..
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_ints.h"
#include "driverlib/interrupt.h"
#include "driverlib/timer.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "driverlib/adc.h"
#include "inc/lm4f120h5qr.h"
#include "utils/uartstdio.h"
#include "led_task.h"
#include "switch_task.h"
#include "routine_task.h"
#include "dht_task.h"
#include "qei_task.h"
#include "lm393_adc.h"
#include "FreeRTOS.h"
#include "task.h"
#include "queue.h"
#include "semphr.h"
#include "driverlib/qei.h"
#include "driverlib/pwm.h"
#include "pwm_task.h"
#include "inc/hw_i2c.h"
#include "driverlib/i2c.h"
#include "display/oled.h"
xSemaphoreHandle g_pUARTSemaphore;
xSemaphoreHandle xCountingSemaphore;
xSemaphoreHandle rCountingSemaphore;
#ifdef DEBUG
void
__error__(char *pcFilename, unsigned long ulLine)
{
}
#endif
void
vApplicationStackOverflowHook(xTaskHandle *pxTask, signed char *pcTaskName)
{
while(1)
{
}
}
// Set I2C : 0 : MASTER
void I2C_init(void){
GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_3);
GPIOPinTypeI2CSCL(GPIO_PORTB_BASE, GPIO_PIN_2);
GPIOPinConfigure(GPIO_PB3_I2C0SDA);
GPIOPinConfigure(GPIO_PB2_I2C0SCL);
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);
SysCtlPeripheralReset(SYSCTL_PERIPH_I2C0);
I2CMasterInitExpClk(I2C0_MASTER_BASE, SysCtlClockGet(), true);
}
int
main(void)
{
ROM_SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ |
SYSCTL_OSC_MAIN);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD); //for DHT
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA); //for UART
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB); //for I2C
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC); //for QEI1
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_QEI1);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE); //for ADC
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0); //for Timer 0
GPIOPinConfigure(GPIO_PC5_PHA1); //Quadrature Encoder
GPIOPinConfigure(GPIO_PC6_PHB1);
GPIOPinTypeQEI(GPIO_PORTC_BASE, GPIO_PIN_5 | GPIO_PIN_6);
//QEIDisable(QEI1_BASE);
//QEIIntDisable(QEI1_BASE,QEI_INTERROR | QEI_INTDIR | QEI_INTTIMER | QEI_INTINDEX);
// Configure quadrature encoder
//QEIConfigure(QEI1_BASE, (QEI_CONFIG_CAPTURE_A_B | QEI_CONFIG_NO_RESET | QEI_CONFIG_QUADRATURE | QEI_CONFIG_NO_SWAP), 23);
// Enable the quadrature encoder.
//QEIEnable(QEI1_BASE);
//Set position to a middle value so we can see if things are working
//QEIPositionSet(QEI1_BASE, 0);
GPIOPinConfigure(GPIO_PA0_U0RX); //UART
GPIOPinConfigure(GPIO_PA1_U0TX);
ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
UARTStdioInit(0);
//ADC
GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_3);
SysCtlADCSpeedSet(SYSCTL_ADCSPEED_250KSPS);
ADCHardwareOversampleConfigure(ADC0_BASE, 64);
ADCSequenceDisable(ADC0_BASE, 1);
ADCSequenceConfigure(ADC0_BASE, 0, ADC_TRIGGER_PROCESSOR, 0);
ADCSequenceStepConfigure(ADC0_BASE, 0,0, ADC_CTL_CH0);
ADCSequenceEnable(ADC0_BASE,0);
I2C_init();
Display_Boot();
PWM_init(50);
UARTprintf("\n\nWelcome to the Stellaris EK-LM4F120 FreeRTOS Demo!\n");
g_pUARTSemaphore = xSemaphoreCreateMutex();
xCountingSemaphore = xSemaphoreCreateCounting(50,0); //for interrupt semaphore in dht_task
rCountingSemaphore = xSemaphoreCreateCounting(10,0); //for interrupt semaphore in routine_task
// Create Tasks.
if(LEDTaskInit() != 0){while(1){}} //LED
if(SwitchTaskInit() != 0){while(1){}} //SWITCH
if(xCountingSemaphore != NULL){
if(DHTTaskInit() != 0){while(1){}} //DHT
}else{
UARTprintf("failed to create counting semaphore");
}
//if(LM393TaskInit() != 0){while(1){}}
if(RoutineTaskInit() != 0){while(1){}}
//if(QeiTaskInit() != 0){while(1){}}
vTaskStartScheduler();
while(1)
{
}
}