Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137 HALCOGEN Vs. iotms570LS3137zwt.h

Other Parts Discussed in Thread: TMS570LS3137, HALCOGEN

Hello,

I´m using HALCOGEN to create Drivers for the internal devices of the TMS570LS3137.

But we want to change this to use the iotms570LS3137zwt.h Header.

Now the problem is, when I use the HALCOGEN File for controlling the I2C device I get the following assembler output when I want to put the device out of reset:

C-Code: ((i2cBASE_t *)0xFFF7D400U)->MDR |= I2C_RESET_OUT;

Assembler Code:
   
      0x2d67c: 0xe59f01e8      LDR         R0, ??DataTable16       ; I2CMDR
      0x2d680: 0xe5900000     LDR         R0, [R0]
      0x2d684: 0xe3900020     ORRS      R0, R0, #32                   ; 0x20
      0x2d688: 0xe59f11dc      LDR         R1, ??DataTable16       ; I2CMDR
      0x2d68c: 0xe5810000     STR         R0, [R1]
  

So, now when I use the iotms570LS3137zwt.h Header I use the following Command:

C-Code: I2CMDR |= I2C_RESET_OUT;

Assembler Code:


      0x2d690: 0xe59f01d4      LDR         R0, ??DataTable16       ; I2CMDR
      0x2d694: 0xe1d000b0     LDRH       R0, [R0]
      0x2d698: 0xe3900020     ORRS      R0, R0, #32                   ; 0x20
      0x2d69c: 0xe59f11c8       LDR         R1, ??DataTable16       ; I2CMDR
      0x2d6a0: 0xe1c100b0     STRH       R0, [R1]

Now, can you please tell me why the 2 Assembler outputs are different?

When I use HALCOGEN => it works.

When I use the Header => it doesn´t work.

PS: I´m using HALCOGEN Version 3.05.00, Header Revision Nr.  57770

Thanks.

David


  

  • Thank you for using the Hercules forum. One of our engineers will be with you shortly. 

  • David,

    I don't have the header that you're referencing (iotms570LS3137zwt.h) handy - actually not sure which package this came from. 

    But looking at the generated code, I see that the 2nd example is using LDRH and STRH instructions to access the I2CMDR register.  These are 16-bit reads and writes (which might make some sense as I belive the I2C peripheral is natively a 16-bit peripheral).   On the other hand, the HalCoGen header has this address declared as a 32-bit register.

    Let me know where to find the iomtms...h file and we can check it or if you want to check it, I suspect it could be an issue of endian.   The address 0x24 which is 32-bit aligned in the header file from HalCoGen is endian independent.  But if you use a 16-bit aligned address, I'm pretty sure it would need to change to 0x26 because the bits of the register appear to be on the lower 16-bits of the word which is offset +2 for a big endian device.  (for a little endian part like RM48 I think it would be still ok as 0x24...)

     

  • Hi Anthony,

    Thanks for your reply.

    I´ve attached the header file in this post now (It´s out of the IAR Workbench).

    So, what is the right way to work with a 16Bit register in this machine. Should I use 16Bit or 32Bit values with this Registers?

    1411.iotms570LS3137zwt.h

    Greetings

    David

  • David,

    You can use either.  The problem I believe is that the address is wrong for the big endian TMS570, in this line of code (Line 15344)

    __IO_REG16_BIT(I2CMDR,          0xFFF7D424,__READ_WRITE ,__i2cmdr_bits);

    The TMS570 is big endian (BE-32).   So the lower 16 bits of a 32-bit bus are address +0x2 and the upper are address +0x00.

    Try adding +2 to the addresses in your header that are _IO_REG16_BIT and see if this helps.  They all look wrong to me.

    If these were changed to 32-bit entities, then the addresses would be fine.