This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RE: Blinky LED example - stuck in _memoryInit_ loop

Hi,

Just to add a little bit more information.

We have been seeing exactly the same issues for the last year now.  It happens on our development boards 10-20 times a day, however only when debugging.

When the application is executed from power-on-reset we have never seen this issue in >1K reset tests without the debugger connected.

We are using XDS100V2 debuggers from SpectrumDigital.  Sometimes the debugger complains about stale breakpoint op-codes stuck in memory.  Maybe this has something to do with it?

Thanks

Stomp!

 

EDIT:  Split from post http://e2e.ti.com/support/microcontrollers/hercules/f/312/t/205959.aspx which was CLOSED.

Didn't want the new question to get lost at the end of a Closed posting.  -Anthony Seely