This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C Sleep and Deep Sleep Power Configuration



Tool set: CCS v 5.3

MCU: TM4C1230

Board: Custom

How does one set the Sleep and Deep Sleep Power Configuration for FLASH and SRAM using either the peripheral API or ROM API? Requires write access to SYS CONTROL register 18, SLPPWRCFG and register 19 DSLPPWRCFG.

  • Hello Scott,

    You can use the API's SysCtlDeepSleepPowerSet and SysCtlSleepPowerSet to configure the Deep Sleep and Sleep Power Config register

    Regards

    Amit Ashara

  • Which API am I to use for these functions, they are not in my sysctl.h

  • Hello Scott,

    Which version of TIVAWare release are you using

    Regards

    Amit Ashara

  • TivaWare_C_Series-1.1

  • Hello Scott

    The function API's are in there in the latest release. You may want to update to TivaWare_C_Series-2.0.1.11577

    In case there is a specific reason not to use it, I would suggest to still download the same and keep it for reference to API's in the immediate future.

    Regards

    Amit Ashara

  • is that part of the update list above (generated by CCS check for updates) or do I have to go to a specific url.

    Is it a seamless update, will my ccs project add the new path to my project search paths?

  • Is 2.0.1.1xxx part of the list included in my "paste"?

    Is it a seamless update, that is will my project search paths be updated also?

  • Hello Scott,

    No. It was TIVAWare 1.1 in the previous post. I am not sure if CCS gets the update, so you have to go to the TIVA web page

    http://www.ti.com/lsds/ti/microcontroller/tiva_arm_cortex/c_series/tools_software.page

    The API's should be a seamless update but paths may need to be worked

    Regards

    Amit Ashara

  • I went to the url and downloaded the latest Tiva Ware driver library.

    I ran the *.exe and it has created and loaded files into c:\ti\TivaWare_C_Series-2.0.1.11577.

    I noticed the new directory is subset of the previous, TivaWare_C_Series-1.1.

    How do manage resources from these two sources on a project.

    Should I upgrade the entire TivaWare package to 2.0.1.11577?

  • Hello Scott,

    Yes, my suggestion would be to upgrade to the new package.

    Regards

    Amit Ashara

  • Thanks for your help.

  • Device: TM4C1230H

    Tiva Ware C Series 2.0.1.11577

    use: SysCtlDeepSleepPowerSet(SYSCTL_FLASH_LOW_POWER | SYSCTL_SRAM_LOW_POWER);

    sysclt.c API: specifies param ui32Config as logical or of

    SYSCTL_FLASH_NORMAL

    SYSCTL_FLASH_LOW_POWER

    SYSCTL_SRAM_NORMAL

    SYSCTL_SRAM_STANDBY

    SYSCTL_SRAM_LOW_POWER

    However, these input parameters are NOT DEFINED anywhere in Tiva Ware C Series 2.0.1.11577.

    Where are they?

  • They are in the next release, these were unfortunately omitted from previous releases. 

    Here are the definitions if you need them before the next TivaWare release is out.

    //*****************************************************************************
    //
    // The following are values that can be passed to the SysCtlSleepPowerSet() and
    // SysCtlDeepSleepPowerSet() APIs as the ui32Config parameter.
    //
    //*****************************************************************************
    #define SYSCTL_LDO_SLEEP        0x00000200  // LDO in sleep mode
                                                // (Deep Sleep Only)
    #define SYSCTL_TEMP_LOW_POWER   0x00000100  // Temp sensor in low power mode
                                                // (Deep Sleep Only)
    #define SYSCTL_FLASH_NORMAL     0x00000000  // Flash in normal mode
    #define SYSCTL_FLASH_LOW_POWER  0x00000020  // Flash in low power mode
    #define SYSCTL_SRAM_NORMAL      0x00000000  // SRAM in normal mode
    #define SYSCTL_SRAM_STANDBY     0x00000001  // SRAM in standby mode
    #define SYSCTL_SRAM_LOW_POWER   0x00000003  // SRAM in low power mode

  • Can you help me understand why I am only able to reduce current draw to 8.9mA when entering DEEP SLEEP using the following API's:

    // Configuration for SHUT DOWN

    //====================

    // Peripherals

    // Sleep and Deep Sleep clock gating enabled, ROM_SysCtlPeripheralClockGating(1);

    // ROM_SysCtlPeripheralDeepSleepDisable() for all known peripherals

    Proj_Peripheral_Config_ShutDown();

    //====================

    //====================

    // ROM_SysCtlPeripheralPowerOff() for all known peripherals

    //Proj_Peripheral_PowerOff();

    //====================

    //====================

    // LDO voltage in DEEP SLEEP

    SysCtlLDODeepSleepSet(SYSCTL_LDO_0_90V);

    //====================

    //====================

    // SRAM and FLASH modes in DEEP SLEEP

    SysCtlDeepSleepPowerSet(SYSCTL_LDO_SLEEP | SYSCTL_TEMP_LOW_POWER | SYSCTL_FLASH_LOW_POWER | SYSCTL_SRAM_LOW_POWER);

    //SysCtlDeepSleepPowerSet(SYSCTL_FLASH_LOW_POWER | SYSCTL_SRAM_LOW_POWER);

    //====================

    // NOT present in sysctl.c or ROM driver api

    // SysCtlLPCLowPowerConfigSet(SYSCTL_LPCLPWR_SRAM_OFF);

    //====================

    // power down clock in DEEP SLEEP

    SysCtlDeepSleepClockConfigSet(SYSCTL_DSLP_DIV_64, SYSCTL_DSLP_PIOSC_PD);

    //====================

    // SHUT DOWN mode, only a hardware reset can restore operation

    while (1)

    {

        SysCtlDeepSleep();

        SysCtlDelay(100);

    }

  • Hi Scott,

    Can you confirm the following

    1. In the function Proj_Peripheral_Config_ShutDown(); you are setting-clearint the Deep Sleep Clock Enable for the peripherals.

    2. In the same function you are setting SysCtlPeripheralClockGating(true)

    3. The Deep Sleep Clock Source is being set as MOSC

    4. The debugger is disconnected (not just disconnect from the CCS window). The Debug Enable is a sticky bit in CM4. One sure shot way is to remove the power and then connect back the power

    Regards

    Amit

  • Hello Amit,

    Regarding (1):

    Sample code from Proj_Peripheral_Config_ShutDown():

    void Proj_Peripheral_Config_ShutDown(void)

    {

        ROM_SysCtlPeripheralClockGating(1);

         //============================================================

         // all peripherals disabled during SHUT DOWN

        ROM_SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_ADC0);

        ROM_SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_ADC1);

        ROM_SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_CAN0);

        ... repeated for all known peripherals in TM4C1230

    }

    Not sure what API you are referring to "Deep Sleep Clock Enable".

    Regarding (3):

    In Main.c, I set:

    ROM_SysCtlMOSCConfigSet(SYSCTL_MOSC_NO_XTAL);

    ROM_SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_INT | SYSCTL_MAIN_OSC_DIS);

    // Set the system clock for DEEP SLEEP operation.

    // Precision internal oscillator (i.e. SYSCTL_SYSDIV_1).

    ROM_SysCtlDeepSleepClockSet(SYSCTL_DSLP_DIV_1 | SYSCTL_DSLP_OSC_INT);

    In the preparation for SHUT DOWN of my application (shown previously), I set:

    // power down clock in DEEP SLEEP

    SysCtlDeepSleepClockConfigSet(SYSCTL_DSLP_DIV_64, SYSCTL_DSLP_PIOSC_PD);

    Regarding (4):

    The SHUT DOWN current draw is 10+ mA with ICD connected. After disconnecting ICD and resetting my target,

    the SHUT DOWN current draw is 8.9mA.

  • Hi Scott,

    So #1 and #2 are taken care by the Proj_Peripheral_Config_ShutDown function call.

    For #3, the second API SysCtlDeepSleepClockConfigSet is overwriting the first API. an you put a break point at SysCtlDeepSleep and check the value of the System Control register DSLPCLKCFG?

    Secondly you want to set the deep sleep clock source as PIOSC in the ROM_SysCtlDeepSleepClockSet and later in the SysCtlDeepSleepClockConfigSet you are requesting it to be Powered Down. This is a conflicting condition.

    Regards

    Amit Ashara

  • The application has three possible modes:

    a. running - process pending project events

    b. DEEP SLEEP - no project events pending, enable minimum set of peripherals and interrupts, wait for interrupt

    c. SHUT DOWN - a forced event/command, halt all activity, enter MINIMUM current draw, RESET required to exit

    Modes (a) and (b) are alternating continuously. Mode (c) is entered only after a command.

    The program flow (and my intention) is as follows:

    Main.c sets normal operating conditions of:

    1. no MOSC xtal

    2. System Clock = PIOSC at 16.0MHz

    3. Deep Sleep system clock = PIOSC at 16.0MHz

    4. call Proj_Peripheral_Config_DeepSleep(), enables a minimum set of peripherals

    5. Configure project GPIO, WDOG 0, SysTick, Timers, UARTS, SSI, ADC, ...

    6. call Loop.c

    Loop.c (the ROOT or IDLE task/thread)

    if (project event)

    {

        // process event, event function calls may result in a new event, enabled interrupt, etc.

    }

    else if (test for project command to force SHUT DOWN)

    {  

        // ALL pending events must be processed before executing SHUT DOWN.

        // THIS MODE is intended to draw the ABSOLUTE minimum current.

        // RESET required to exit.

        // Yes, I am trying to reconfigure elements of DEEP SLEEP 

        // for the SPECIAL condition of SHUT DOWN. 

     

        // IT ALSO MAKES SENSE TO ME TO DISABLE MOST INTERRUPTS, BUT SO FAR THIS

        // HAS YIELDED ERRATIC RESULTS IN CURRENT DRAW, WDOG RESETS, AND FAULTS

       

        // set peripheral config for SHUT DOWN,

        Proj_Peripheral_Config_ShutDown();

        // set LDO Deep Sleep voltage

        SysCtlLDODeepSleepSet(SYSCTL_LDO_0_90V);

        // set SRAM and FLASH Deep Sleep modes

       SysCtlDeepSleepPowerSet(SYSCTL_LDO_SLEEP | 

            SYSCTL_TEMP_LOW_POWER  |  

            SYSCTL_FLASH_LOW_POWER |

            SYSCTL_SRAM_LOW_POWER);

        // set Deep Sleep Clock for power down

        SysCtlDeepSleepClockConfigSet(SYSCTL_DSLP_DIV_64, SYSCTL_DSLP_PIOSC_PD);

        // enter and remain in Deep Sleep until hardware RESET

        while (1)

        {

            SysCtlDeepSleep();

            SysCtlDelay(100);

        }

    }

    else (opportunity to enter DEEP SLEEP, i.e. no pending project events)

    {

        // I will probably have MORE QUESTIONS here, but my goal would be enter minimum current draw

        // for my minimum set of peripherals and interrupts enabled

        // as set in Main.c

    }

  • Hi Scott,

    Everything is correct except the following should not be called for TM4C123

    SysCtlDeepSleepClockConfigSet(SYSCTL_DSLP_DIV_64, SYSCTL_DSLP_PIOSC_PD);

    I can try the configuration you have already given to co-relate to the current you have mentioned. Please note that I will assume that no peripheral is to be clocked in deep sleep mode!!! I should have data tomorrow.

    Also another factor is the IO's connected to other devices. If they are in output mode and are driven high in idle state, they could be sourcing current from TM4C123 to other devices, causing the current to be higher as well. Could you check that as well

    Regards,

    Amit Ashara

  • According to page 244 of the Tm4C1230H data sheet,

    PIOSCPD: 0x00000002 - is a bit set in the Deep Sleep Clock Configuration register (base 0x400Fe000, offset 0x144) that allows the PIOSC to be powered down during DEEP SLEEP.

    SysCtlDeepSleepClockConfig(): uses

    if(CLASS_IS_BLIZZARD)

    {

    //

    // Set the deep-sleep clock configuration.

    //

    HWREG(SYSCTL_DSLPCLKCFG) = (ui32Config & ~SYSCTL_DSLPCLKCFG_D_M) |

    ((ui32Div - 1) << SYSCTL_DSLPCLKCFG_D_S);

    }

    else

    {

    //

    // Set the PIOSC power down bit.

    //

    if(ui32Config & SYSCTL_DSLP_PIOSC_PD)

    {

    ui32Value |= SYSCTL_DSCLKCFG_PIOSCPD;

    }

    //

    // Update the deep-sleep clock configuration.

    //

    HWREG(SYSCTL_DSCLKCFG) = ui32Value;

    where;

    #define SYSCTL_DSCLKCFG_PIOSCPD 0x80000000 // PIOSC Power Down

    #define SYSCTL_DSCLKCFG 0x400FE144 // Deep Sleep Clock Configuration

    so I see a difference between the data sheet bit position (0x00000002) and the #define 0x80000000.

    Do I need to use  HWREG(SYSCTL_DSCLKCFG) |= 0x00000002; ????

  • How do I achieve the IDD DEEP SLEEP current of 1mA that is published in the TM4C1230H data sheet???

  • Hi Scott,

    As I mentioned earlier, please remove the line containing the API

    SysCtlDeepSleepClockConfigSet(SYSCTL_DSLP_DIV_64, SYSCTL_DSLP_PIOSC_PD);

    Instead use

    SysCtlDeepSleepClockSet(SYSCTL_DSLP_DIV_1|SYSCTL_DSLP_OSC_INT30|SYSCTL_DSLP_PIOSC_PD);

    This will make the device enter deep sleep with 30KHz LFIOSC. If you check the current consumtion table in the electrical specification the 1mA current is for FLASHPM=0x2, Peripheral all OFF and clock as 30KHz LFIOSC with LDO at 1.2V.

    I would be needing some additional data. Please put a break point on the function SysCtlDeepSleep and then publish the content of the following system control registers

    SYSCTL.RCC

    SYSCTL.DSLPCLKCFG

    SYSCTL.DSPLPWRCFG

    SYSCTL.LDODPCTL

    SYSCTL registers from offset 0x800 to 0x85C

    Regards

    Amit Ashara

  • inserting file, I am tired of this input window

    // CODE FOR SHUT DOWN
    	// Configuration for SHUT DOWN
    
    	//====================
    	// Peripherals
    	// Sleep and Deep Sleep clock gating enabled, ROM_SysCtlPeripheralClockGating(1);
    	// ROM_SysCtlPeripheralDeepSleepDisable() for all known peripherals
    	Proj_Peripheral_Config_ShutDown();
    	//====================
    
    	//====================
    	// ROM_SysCtlPeripheralPowerOff() for all known peripherals
    	//Proj_Peripheral_PowerOff();
    	//====================
    
    	//====================
    	// LDO voltage in DEEP SLEEP
    	SysCtlLDODeepSleepSet(SYSCTL_LDO_0_90V);
    	//====================
    
    	//====================
    	// SRAM and FLASH modes in DEEP SLEEP
    	SysCtlDeepSleepPowerSet(SYSCTL_LDO_SLEEP | SYSCTL_TEMP_LOW_POWER | SYSCTL_FLASH_LOW_POWER | SYSCTL_SRAM_LOW_POWER);
    	//SysCtlDeepSleepPowerSet(SYSCTL_FLASH_LOW_POWER | SYSCTL_SRAM_LOW_POWER);
    	//====================
    
    	// NOT present in sysctl.c or ROM driver api
    	// SysCtlLPCLowPowerConfigSet(SYSCTL_LPCLPWR_SRAM_OFF);
    
    	//====================
    	// clock in DEEP SLEEP
    	SysCtlDeepSleepClockSet(SYSCTL_DSLP_DIV_1 | SYSCTL_DSLP_OSC_INT30 | SYSCTL_DSLP_PIOSC_PD);
    	//====================
    
    	// SHUT DOWN mode, only a hardware reset can restore operation
    	while (1)
    	{
    		SysCtlDeepSleep();
    		SysCtlDelay(100);
    	}
    
    // ISSUEING SHUTDOWN COMMAND
    
    	[C],VERSION,2nd Gen GPSC MOBILE V0.067 02-11-2014,(c)RSC.
    	MOBILE> ,1388,0.067,16000000,0,32,64,96,128,160,192,224,0x00000000
    	MOBILE>
    	[N],StopNav,0
    
    	MOBILE>
    	MOBILE> SHUTDOWN
    	[C],SHUTDOWN
    
    	[N],StopNav,1
    
    	SHUTDOWN
    
    // Current draw when 8.37mA
    
    //Register Dump in  SysCtlDeepSleep()
    
    RCC (0x400FE050)		00000000
    DSLPCLKCFG (0x400FE144)	00000032
    DSPLPWRCFG (can't find this register in data sheet or API, can you provide)
    LDODPCTL (can't find this register in data sheet or API, can you provide)
    
    SYSCTL registers from offset 0x800 to 0x85C
    #define SYSCTL_DCGCWD           0x400FE800  // Watchdog Timer Deep-Sleep Mode
    
    ADDRESS		DATA
    0x400FE800	00000000	00000000	00000000	00000000	00000000	00000001	00000000	00000000
    
    0x400FE820	00000000	00000000	00000000	00000000	00000000	00000000	00000000	00000000
    
    0x400FE840	00000000	00000000	00000000	00000000	00000000	00000000	00000000	00000000
    
    0x400FE860	00000000	00000000	00000000	00000000	00000000	00000000	00000000	00000000
    
    

  • For lowest current:

    If I have GPIOs configure as outputs, is it sufficient to set them low or do I need to reconfigure as an input.

    What about pins used by peripherals: UART0, UART2, and SSI1? Do I need to change any of these?

  • The following is from sysctl.c.

    It states "

    //! This function allows the power to a peripheral to be turned off. The

    //! peripheral continues to receive power when its clock is enabled, but

    //! the power is removed when its clock is disabled.

    "

    How does one disable the clock to a peripheral in the TM4C1230???????????

    //*****************************************************************************

    //

    //! Powers off a peripheral.

    //!

    //! \param ui32Peripheral is the peripheral to be powered off.

    //!

    //! This function allows the power to a peripheral to be turned off. The

    //! peripheral continues to receive power when its clock is enabled, but

    //! the power is removed when its clock is disabled.

    //!

    //! The \e ui32Peripheral parameter must be only one of the following values:

    //! \b SYSCTL_PERIPH_ADC0, \b SYSCTL_PERIPH_ADC1, \b SYSCTL_PERIPH_CAN0,

    //! \b SYSCTL_PERIPH_CAN1, \b SYSCTL_PERIPH_CAN2, \b SYSCTL_PERIPH_COMP0,

    //! \b SYSCTL_PERIPH_COMP1, \b SYSCTL_PERIPH_COMP2, \b SYSCTL_PERIPH_EEPROM0,

    //! \b SYSCTL_PERIPH_EPI0, \b SYSCTL_PERIPH_FAN0, \b SYSCTL_PERIPH_FAN1,

    //! \b SYSCTL_PERIPH_GPIOA, \b SYSCTL_PERIPH_GPIOB, \b SYSCTL_PERIPH_GPIOC,

    //! \b SYSCTL_PERIPH_GPIOD, \b SYSCTL_PERIPH_GPIOE, \b SYSCTL_PERIPH_GPIOF,

    //! \b SYSCTL_PERIPH_GPIOG, \b SYSCTL_PERIPH_GPIOH, \b SYSCTL_PERIPH_GPIOJ,

    //! \b SYSCTL_PERIPH_GPIOK, \b SYSCTL_PERIPH_GPIOL, \b SYSCTL_PERIPH_GPIOM,

    //! \b SYSCTL_PERIPH_GPION, \b SYSCTL_PERIPH_GPIOP, \b SYSCTL_PERIPH_GPIOQ,

    //! \b SYSCTL_PERIPH_HIBERNATE, \b SYSCTL_PERIPH_I2C0, \b SYSCTL_PERIPH_I2C1,

    //! \b SYSCTL_PERIPH_I2C2, \b SYSCTL_PERIPH_I2C3, \b SYSCTL_PERIPH_I2C4,

    //! \b SYSCTL_PERIPH_I2C5, \b SYSCTL_PERIPH_PWM0, \b SYSCTL_PERIPH_PWM1,

    //! \b SYSCTL_PERIPH_QEI0, \b SYSCTL_PERIPH_QEI1, \b SYSCTL_PERIPH_SSI0,

    //! \b SYSCTL_PERIPH_SSI1, \b SYSCTL_PERIPH_SSI2, \b SYSCTL_PERIPH_SSI3,

    //! \b SYSCTL_PERIPH_TIMER0, \b SYSCTL_PERIPH_TIMER1, \b SYSCTL_PERIPH_TIMER2,

    //! \b SYSCTL_PERIPH_TIMER3, \b SYSCTL_PERIPH_TIMER4, \b SYSCTL_PERIPH_TIMER5,

    //! \b SYSCTL_PERIPH_UART0, \b SYSCTL_PERIPH_UART1, \b SYSCTL_PERIPH_UART2,

    //! \b SYSCTL_PERIPH_UART3, \b SYSCTL_PERIPH_UART4, \b SYSCTL_PERIPH_UART5,

    //! \b SYSCTL_PERIPH_UART6, \b SYSCTL_PERIPH_UART7, \b SYSCTL_PERIPH_UDMA,

    //! \b SYSCTL_PERIPH_USB0, \b SYSCTL_PERIPH_WDOG0, \b SYSCTL_PERIPH_WDOG1,

    //! \b SYSCTL_PERIPH_WTIMER0, \b SYSCTL_PERIPH_WTIMER1,

    //! \b SYSCTL_PERIPH_WTIMER2, \b SYSCTL_PERIPH_WTIMER3,

    //! \b SYSCTL_PERIPH_WTIMER4, or \b SYSCTL_PERIPH_WTIMER5.

    //!

    //! \note The ability to power off a peripheral varies based on the Tiva

    //! part in use. Please consult the data sheet for the part you are using to

    //! determine if this feature is available.

    //!

    //! \return None.

    //

    //*****************************************************************************

    void

    SysCtlPeripheralPowerOff(uint32_t ui32Peripheral)

    {

  • Hello Scott,

    Thanks for the register dump. The issue could not be isolated because of the following

    1. RCC register offset is 0x060 and not 0x050 so a new dump would be needed

    2. The DSLPPWRCFG offset is 0x18C, LDODPCTL offset is 0x1BC. It is there in the data sheet, so you may have to check which version of the data sheet you are using. I have the November-2013 version.

    3. The DCGC registers and DSLPCLKCFG register look all OK.

    Driving them low should be OK. If in deep sleep the only method to come back in Run State is to reset the device, my suggestion would be to put all IO's in input state with pull downs enabled.

    Regards

    Amit Ashara

  • Hi Scott,

    Clock to a peripheral id disabled by the API SysCtlPeripheralDisable

    All the API's are documented in the TIVAWare Peripheral Driver User Guide.

    Regards

    Amit Ashara

  • Hi Scott,

    I made a small code to run the following example

    SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_XTAL_16MHZ |
                       SYSCTL_OSC_INT);

    SysCtlPeripheralClockGating(1);
        SysCtlDeepSleepClockSet(SYSCTL_DSLP_DIV_1|SYSCTL_DSLP_OSC_INT30|SYSCTL_DSLP_PIOSC_PD);

    SysCtlLDODeepSleepSet(SYSCTL_LDO_0_90V);

    SysCtlDeepSleepPowerSet(SYSCTL_FLASH_LOW_POWER | SYSCTL_SRAM_LOW_POWER);

    SysCtlDeepSleep();

    and measured the current.to be ~0.5mA. This is less than 1.0mA as shown in the data sheet as the LDO voltage has been scaled to 0.9V instead of the operational 1.2V

    Regards

    Amit Ashara

  • Amit,

    see attachment for new code and register dump.

    // 20140213sm CODE FOR SHUT DOWN
    
    			if (_Device_Control.dwEvent & (EVENT_SHUT_DOWN_WAKEUP | EVENT_SHUT_DOWN))
    			{
    				if (_Device_Control.ucCountDownToShutDown == 0)
    				{
    					WriteString(_Device_Control.ucASCIIPortIO, (UCHAR *) pCRLF);
    					WriteString(_Device_Control.ucASCIIPortIO, (UCHAR *) pSHUT_DOWN);
    					WriteString(_Device_Control.ucASCIIPortIO, (UCHAR *) pCRLF);
    
    					//====================
    					// IO pins
    					LEDsOFF();
    					TURN_TONE_OFF();
    					// TxRx - should already be in power down state
    					bTemp = RSC_FALSE;
    					bTemp = TxRx_PowerDown();
    					SysCtlDelay(1000000);
    					//SSI1_DRIVE_FSS_INACTIVE;
    					//CC1120_DEASSERT_CS;
    
    					if (_Device_Control.dwEvent & EVENT_SHUT_DOWN_WAKEUP)
    					{
    						_Device_Control.dwEvent = 0;
    						// shut down, leave only motion interrupt enabled
    
    					}
    					else	// _Device_Control.dwEvent == EVENT_SHUT_DOWN
    					{
    						_Device_Control.dwEvent = 0;
    
    						//********************************
    						// Configuration for SHUT DOWN
    						//********************************
    
    						//====================
    						// LDO voltage in DEEP SLEEP
    						// 0.9V results in lower current draw
    					    	SysCtlLDODeepSleepSet(SYSCTL_LDO_0_90V);
    					    	//SysCtlLDODeepSleepSet(SYSCTL_LDO_1_20V);
    						//====================
    
    						//====================
    						// SRAM and FLASH modes in DEEP SLEEP
    						//
    					    	// NOTE:  MAKES NO DIFFERENCE WHICH CALL IS MADE
    						//
    					    	//SysCtlDeepSleepPowerSet(SYSCTL_LDO_SLEEP | SYSCTL_TEMP_LOW_POWER | SYSCTL_FLASH_LOW_POWER | SYSCTL_SRAM_LOW_POWER);
    					    	SysCtlDeepSleepPowerSet(SYSCTL_FLASH_LOW_POWER | SYSCTL_SRAM_LOW_POWER);
    						//====================
    
    						//====================
    						// clock in DEEP SLEEP
    					    	SysCtlDeepSleepClockSet(SYSCTL_DSLP_DIV_1 | SYSCTL_DSLP_OSC_INT30 | SYSCTL_DSLP_PIOSC_PD);
    						//====================
    
    						//====================
    						// Peripherals
    						// SysCtlPeripheralClockGating(1);
    					    	// SysCtlPeripheralDeepSleepDisable() for all project peripherals
    						// SysCtlPeripheralDisable() for all project peripherals
    					    	Proj_Peripheral_Config_ShutDown();
    						//====================
    
    					    	// SHUT DOWN mode, only a hardware reset can restore operation
    						//
    					    	// NOTE:  20140213sm: on a target board NOT connected to any UART or ICD, the SHUT DOWN current = 2.2mA
    						//
    						while (1)
    						{
    							SysCtlDeepSleep();
    							SysCtlDelay(1);
    						}
    					}
    
    // 20140213sm Proj_Peripheral_Config_ShutDown() function call
    
    //============================================================
    // Description:
    //
    // SHUT DOWN configuration for all project peripherals.
    //============================================================
    void Proj_Peripheral_Config_ShutDown(void)
    {
    
    	//============================================================
        	// project peripherals without a #define for a call to
    	// SysCtlPeripheralDeepSleepDisable().
    	
    	ROM_SysTickIntDisable();
    	ROM_SysTickDisable();
        	ROM_FPUDisable();
    
    	SysCtlPeripheralClockGating(RSC_TRUE);
    
    	//============================================================
        	// all project peripherals are disabled during SHUT DOWN
    	
    	SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_WDOG0);
    	SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_TIMER1);
    	SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_TIMER2);
    	SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_SSI1);
    	SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_ADC0);
    	SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_UART0);
    	SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_UART2);
    
    	SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOA);
    	SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOB);
    	SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOC);
    	SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOD);
    	SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOE);
    	SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOF);
    	SysCtlPeripheralDeepSleepDisable(SYSCTL_PERIPH_GPIOG);
    
    	//============================================================
        	// NOTE: DOES anything need to be done for NON project peripherals?
    }
    
    // ISSUEING SHUTDOWN COMMAND
    
    	[C],VERSION,2nd Gen GPSC MOBILE V0.069 02-13-2014,(c)RSC.
    	MOBILE> ,1388,0.069,16000000,0,32,64,96,128,160,192,224,0x00000000
    	MOBILE>
    	[N],StopNav,0
    
    	MOBILE>
    	MOBILE> SHUTDOWN
    	[C],SHUTDOWN
    
    	[N],StopNav,1
    
    	SHUTDOWN
    
    
    // breakpoint set in SysCtlDeepSleep() at CPUwfi();
    // Current draw, connected to ICD == 8.37mA
    // NOTE:  20140213sm: on a target board NOT connected to any UART or ICD, the SHUT DOWN current = 2.2mA
    
    
    //Register Dump in  SysCtlDeepSleep()
    
    RCC (0x400FE060)			0x0F8E3811
    DSLPCLKCFG (0x400FE144)		0x00000032
    DSPLPWRCFG (0x400FE18C)		0x00000023
    LDODPCTL (0x400FE1BC)		0x80000012
    
    SYSCTL registers from offset 0x800 to 0x85C
    #define SYSCTL_DCGCWD           0x400FE800  // Watchdog Timer Deep-Sleep Mode
    
    ADDRESS		DATA
    0x400FE800	00000000	00000000	00000000	00000000	00000000	00000001	00000000	00000000
    
    0x400FE820	00000000	00000000	00000000	00000000	00000000	00000000	00000000	00000000
    
    0x400FE840	00000000	00000000	00000000	00000000	00000000	00000000	00000000	00000000
    
    0x400FE860	00000000	00000000	00000000	00000000	00000000	00000000	00000000	00000000
    
    
    In void Proj_Peripheral_Config_ShutDown(void),

    // NOTE: DOES anything need to be done for NON project peripherals?

    // breakpoint set in SysCtlDeepSleep() at CPUwfi();
    // Current draw, connected to ICD == 8.37mA
    // NOTE:  20140213sm: on a target board NOT connected to any UART or ICD, the SHUT DOWN current = 2.2mA

    //Register Dump in  SysCtlDeepSleep()

    RCC (0x400FE060)   0x0F8E3811
    DSLPCLKCFG (0x400FE144)  0x00000032
    DSPLPWRCFG (0x400FE18C)  0x00000023
    LDODPCTL (0x400FE1BC)  0x80000012

  • Hello Scott,

    The settings look fine. When no ICDI or UART is connected the Shut Down current is 2.2mA as you mentioned. Is the VDDC Pin on the part at 0.9V?

    Regards

    Amit Ashara

  • Yes the VDDC pin is at 0.9V.

  • Hello Scott,

    Did you try the code I had sent to you earlier. This will help make sure that there is no other component on your DK/EK-TM4C board that is consuming the current.

    Regards

    Amit Ashara

  • 7776.20140214sm Response to Amits code example.docx

    Attached is the only code sample that I have received from you.

  • Hello Scott,

    I am using the internal oscillator but not disabling the XTAL Pads. If you could run the small code in a separate test and let me know the current it would be useful as it takes out any SW component

    Secondly which board are you using. I am not sure of that either

    Regards

    Amit

  • Hello Scott,

    Any update on the same for me to follow up, or is it resolved?

    Regards

    Amit

  • Note: no change in current when NOT using SYSCTL_MAIN_OSC_DIS in ROM_SysCtlClockSet().

    See attached schematic (RSC and TI are under mutual non-disclosure so please do not share). I believe I can account for 2.3 mA current draw (see page 3, TCXO current draw). I consider the issue resolved at this point. Thank you for your help.