Other Parts Discussed in Thread: ASH, LMFLASHPROGRAMMER, UNIFLASH
Hello,
For the past 6 months, my TIVA Launchpad has been running perfectly well. All of a sudden, I am unable to debug the device!!
I get the error, "Unable to connect to the device" and a Frequency error.
I looked online and tried the following :
1. Pull out and plug the board back in.
2. Restart CCS (v5) and try again
3. Use the LM Flash Programmer (got the error "Unable to initialize the device -0 "
4. Try a bulk erase to unlock the device using LM Flash Programmer.
Even then, the error persists.
Further details ;
1. Device drivers are up to date. I checked in device manager.
2. Latest version (1601) of LM FLash Programmer
3. My GPIO pins do not conflict with the JTAG pins.
4. I am using a Windows 8 PC and also tried it in my friend's PC. Still the error persists.
Can someone please help me to resolve this problem? Is my board dead or is there a workaround?
-- Ash