Other Parts Discussed in Thread: SW-DK-TM4C129X, TM4C129XNCZAD
I'm using TM4C129xx and I have a question about the USB I/F.
How I configure the USB an a USB device? - I can't see it at the DS.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SW-DK-TM4C129X, TM4C129XNCZAD
I'm using TM4C129xx and I have a question about the USB I/F.
How I configure the USB an a USB device? - I can't see it at the DS.
TI provides a USB library as part of TivaWare so you don't have to write this level of code from scratch.
Check out examples/boards/dk-tm4c129x/usb_dev_*
Which can be found here http://software-dl.ti.com/tiva-c/SW-DK-TM4C129X/2.0/index_FDS.html
Also, note the paragraph at the beginning of the USB chapter:
Hi Amit,
Was on a break for a while. I will not be using any part of the TI supplied USB stack or Tivaware. It is a port of an open source USB stack with my own device drivers. In that scenario can I upload the USB stack to open source? I will not be sharing the datasheet under NDA.
I am also planning to conduct a training on the USB interface of TM4C129NCPDT. In that case I will have to explain the USB interface from the NDA datasheet to the trainees. How should I go about doing this? Should I ask the trainees to download their copies of the datasheet under NDA for the training? Please advise.
Regards
Diptopal