Hi ,
I am trying to interface eMMC to the RM48. However since 4.3 of the eMMC standard the SPI support has been removed which leaves SD/MMC/SDIO as the only connectivity option. eMMC or Managed NAND are our preferred technologies
As far as I’m aware the RM48 does not have an SDIO module.
Are there any other options for me for connecting the eMMC to the RM48?
An SPI to SDIO Module?
NAND Flash connected to the EMIF?
SPI NAND Flash?
Thanks
Sean