Trying to run "Demo Suite Launcher", it reports: "Demo software not detected on microcontroller. .... Would you like to program the demo software into the microcontroller's flash memory now?"
If I click "Yes", Demo says "Now Programming...", the LP's LED "D8" lights and appears to flicker for a few minutes then goes off and nothing else happens and Demo Suite Launcher has to be killed in task manager.
Every executable in the Safety Demo folder has been set to WinXP SP3 compatibility and "Run as Administrator".
Pressing "POR RESET" does nothing as well.
If I build the project in CCS 5.5, it will work, 'sort of'- LED "D10" lights, but when I try to run the demo it says the firmware is not installed and prompts to install it, even if I close CCS, disconnect the LP, then reconnect the LP and run the Demo.