Other Parts Discussed in Thread: MOTORWARE
Hi,
My task is to implement the BLDC motor control using resolver feedback and Space vector modulation. Also to evaluate the motor control performance.
I found that the hercules TMS570LS controllers are most suitable for my application.
I dont require any gate driver modules as, I am going to evaluate the control performance using emulation kit (using matlab and DSpace) that can receive PWM signals.
Could you please suggest which kit that i can by to implement and evaluate the BLDC motor control performances.
option 1: Developer kit .
Option 2: Control kit ( I doubt that it has limitted peripheral access, that is i cant access CAN and i can only use one of NHET or eTimers etc.)
Option 3: Motor control kit ( as of my knowledge this i doesnt required as this is similar to "option 2 control kit" but with gate driver board and motor
,Option 4: Evaluation kit ( My doubt : whether this is the only kit that i can use for evaluation? cant i do evaluation in developer kit or control kit? what makes is special as a evaluation kit?