This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

jump to application code in bootloader code

Hi,

I am writing a bootloader code for Tiva C series launchpad board which will execute first and will jump to the application code address. Can someone tell me how to do that. Any help and refernce would be appreciated.

  • Hello,
    as in "Cortex™-M4 Devices Generic User Guide" (ARM DUI 0553A):
    on system reset, the vector table is fixed at address 0x00000000. Privileged software can write to
    the VTOR to relocate the vector table start address to a different memory location.
    A good (in my opinion) starting point is in "Stellaris® Boot Loader USER’S GUIDE",
    (TI document SW-BOOTLDR-UG-8555).


    To branch to the application :
    - Set the vector table to the beginning of the app
    - Load the stack pointer from the application's vector table
    - Load the initial PC from the application's vector table and branch to
      the application's entry point.

     as in the  Stellarisware bootLoader example, "bl_startup_ewarm.S"
     
     Finally, see also posts

    http://e2e.ti.com/support/microcontrollers/tiva_arm/f/908/t/317657.aspx

    http://e2e.ti.com/support/microcontrollers/tiva_arm/f/908/t/300316.aspx
     
     Regards,
     Claudio
     

  • Hi

    Can somebody  explain me specifically what changes needs to be done to make this boot loader run and jump to the application for execution? Can i have a small example for that or sequence of steps required ?

    Thanx in advance !!

  • Hi,

    here is an excerpt from TivaWare callApplication() function.


    // Set the vector table to the beginning of the app in flash. HWREG(NVIC_VTABLE) = ui32StartAddr; // Load the stack pointer from the application's vector table. // __asm(" ldr r1, [r0]\n" " mov sp, r1"); // Load the initial PC from the application's vector table and branch to // the application's entry point. // __asm(" ldr r0, [r0, #4]\n" " bx r0\n");

    Hope it helps.

    Regards,

    Claudio