Other Parts Discussed in Thread: TM4C123GH6PM
I am working with capacitive booster pack with TivaC series TM4C123gh6pm development board. I have never worked with this booster pack so I started with an example code of capsense, but after debugging I am able to get only center LED to be switched on and not others. Then I searched out that I can see the output on graph also but I am not getting the software on which I can see. So can you please help me out with that software and its downloading link. And even if I can get some help regarding switching on other 8 led’s because I tried using different combination’s to switch on these led’s and still was not successful.
�m e ��� `�oring data in Flash but never finishes the operation. This causes 0xFF to be written to the .mydata Flash area. This causes all other stored parameters to be erased too.
If you could suggest a full proof circuit for SVS it would be great. Once power failure is detected the controller should remain on for a longer period of time for it to store data in the Flash. Hope to receive a reply soon. This is a urgent requirement from our side.
Regards Atul Bhakay