Other Parts Discussed in Thread: TM4C129XNCZAD, LM4819
Hi again! I'm still using the TM4C129XNCZAD on the DK-TM4C129X connected Development Board. This board has an on-board speaker plus LM4819 amplifier for it.
The pin connected to the input of the amplifier on this board is PB2. PD4 also has to be configured as a GPIO output to pull the chip out of shutdown mode. However, for my testing, I have my scope hooked up to the output of PB2 directly, not after the amp (so the state of PD4 doesn't matter).
Because the designer of this board (for some unknown reason) connected the amp to the T5CCP0 pin instead of a PWM module pin, I have to generate the PWM using the timer module instead. I'm pretty sure my code is correct but I'm still not getting any output. The output on this pin is triggered by the comparator interrupt. This interrupt is working perfectly -- the LED comes on every time it trips. But still no noise.
Again, I'm sure I'm making an elementary mistake. All assistance is greatly appreciated! See my code below:
#include <stdint.h>
#include <stdbool.h>
#include "utils/ustdlib.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/interrupt.h"
#include "driverlib/sysctl.h"
#include "driverlib/pin_map.h"
#include "driverlib/debug.h"
#include "driverlib/adc.h"
#include "driverlib/comp.h"
#include "driverlib/gpio.h"
#include "driverlib/timer.h"
#include "driverlib/hibernate.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
//#include "drivers/pinout.h"
//#include "drivers/sound.h"
void makeSomeNoise(uint32_t ui32currentTone) {
ROM_TimerDisable(TIMER5_BASE, TIMER_A); // make sure timer is off
if(ui32currentTone == 1)
{
// if you're with me!
ROM_TimerLoadSet(TIMER5_BASE, TIMER_A, 6000);
ROM_TimerMatchSet(TIMER5_BASE, TIMER_A, 0);
ROM_TimerEnable(TIMER5_BASE, TIMER_A);
ROM_SysCtlDelay(40000000);
}
if(ui32currentTone == 2)
{
}
if(ui32currentTone == 3)
{
// do nothing, because the sound has been cut
}
}
void PWMInitialize(void)
{
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTD_BASE, GPIO_PIN_4); // pin for enabling LM4819
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER5); // enable timer5
ROM_GPIOPinTypeTimer(GPIO_PORTB_BASE, GPIO_PIN_2);
ROM_GPIOPinConfigure(GPIO_PB2_T5CCP0); // set PB2 as Timer5 output CCP0
ROM_TimerClockSourceSet(TIMER5_BASE, TIMER_CLOCK_SYSTEM);
// ROM_TimerPrescaleSet(TIMER5_BASE, TIMER_A, ) // value between 0 and 255 to act as prescaler of timer
ROM_TimerConfigure(TIMER5_BASE, TIMER_CFG_A_PWM|TIMER_CFG_PERIODIC); // configure timer for half-width PWM
ROM_GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_4, 0x10); // PD4 goes high to activate LM4819 amp
}
void Comp0IntHandler(void)
{
ROM_GPIOPinWrite(GPIO_PORTQ_BASE, GPIO_PIN_7, 0x80); // turn led on
ROM_SysCtlDelay(40000000);
makeSomeNoise(1); // play tone 1
//ROM_SysCtlDelay(40000000);
//makeSomeNoise(2); // play tone 2
//ROM_SysCtlDelay(40000000);
//makeSomeNoise(3); // shut off sounds
ROM_GPIOPinWrite(GPIO_PORTQ_BASE, GPIO_PIN_7, 0x00); // turn led off
ROM_ComparatorIntClear(COMP_BASE, 0);
}
int main(void) {
ROM_SysCtlClockFreqSet(SYSCTL_OSC_INT|SYSCTL_USE_PLL|SYSCTL_CFG_VCO_480, 120000000); // set system clock to 120MHz
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD); // enable port D
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOQ); // enable port Q
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC); // enable port C
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB); // enable port B
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_COMP0); // enable analog comparator 0
PWMInitialize(); // initalize PWM system
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTQ_BASE, GPIO_PIN_4); // set PQ4 to output (Blue LED)
ROM_GPIOPinWrite(GPIO_PORTQ_BASE, GPIO_PIN_7, 0x00); // ensure blue LED is off
ROM_GPIOPinTypeComparator(GPIO_PORTC_BASE, GPIO_PIN_7);
ROM_GPIOPinTypeComparator(GPIO_PORTC_BASE, GPIO_PIN_6);
ROM_ComparatorRefSet(COMP_BASE, COMP_REF_2_0625V); // set reference to 2.0625V
ROM_ComparatorConfigure(COMP_BASE, 0, (COMP_TRIG_NONE|COMP_INT_BOTH|COMP_ASRCP_REF|COMP_OUTPUT_NORMAL)); // configure COMP0
ComparatorIntRegister(COMP_BASE, 0, Comp0IntHandler);
ROM_ComparatorIntEnable(COMP_BASE, 0);
while(1)
{
// twiddle thumbs
}
}