This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Programming in tm4c123gxl evaluation kit

I am using tm4c123gxl evaluation kit. I saw the following lines in a c-program (written for the microcontroller on that board). Can anyone tell me the meaning of the following lines.

#define SYSCTL_RCGC2_R          (*((volatile unsigned long *)0x400FE108))

#define SYSCTL_RCGC2_GPIOF      0x00000020  // port F Clock Gating Control

 

SYSCTL_RCGC2_R |= 0x00000020;     // 1) F clock

delay = SYSCTL_RCGC2_R;           // delay   

What it means by activating clock for a port. 

 

  • Hi Deepak,

    Activating a clock means enabling the clock to the corresponding peripheral. Any peripheral or digital logic performing a function consists of flip flops and flip flops require clock.

    The lines in the code are basically accessing the data at the address 0x0400FE108

    Regards

    Amit