Other Parts Discussed in Thread: HALCOGEN
I am using the RM48 HDK with CCS 5.5 and HALCoGen 3.08.
After resert the program stuck in the while-loop of function "setupPLL()".
If I am using HALCoGen 3.06 the program works.
HALCoGen 3.06 generates the line:
systemREG1->CSDISSET = (1U << 1U) | (1U << 6U);
HALCoGen 3.08 generates the line:
systemREG1->CSDISSET = 0x00000001U | 0x00000040U;
I guess this is a bug in HALCoGen 3.08 and the line should be:
systemREG1->CSDISSET = 0x00000002U | 0x00000040U;
Is this a bug in HALCoGen 3.08?