This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM48x F021 flash API

Hello,

We are running out of Flash Bank 0 and trying to flash Bank 1. We seem to be able to erase fine, but not re-program. When flashing we always fail with register FMSTAT indicating a write timeout (PGM = 1).

To try isolating the problem, I also attempted to write a single byte of data to FB1 using the Flash register interface... and I get the same issue. I'm wondering if someone can give me some insight into what's going on.

Below is the routine I use to flash a single byte to FB1.

void ProgramSingleByte() {
FwpWriteByteAccessorType * oFwpWriteByteAccessor = FWPWRITE_BYTE_ACCESSOR_ADDRESS;

FLASH_CONTROL_REGISTER->Fbprot.u32Register = 1U; /* Disable Level 1 Protection */
/* Enable all sectors of current bank for erase and program. For EEPROM banks with more
than 16 sectors, this must be 0xFFFF */
FLASH_CONTROL_REGISTER->Fbse.u32Register = 0xFFFF;
FLASH_CONTROL_REGISTER->Fbprot.u32Register = 0U; /* Enable Level 1 Protection */
/*Unlock FSM registers for writing */
FLASH_CONTROL_REGISTER->FsmWrEna.u32Register = 0x5U;
/* Set command to "Clear the Status Register" */
FLASH_CONTROL_REGISTER->FsmCommand.FSM_COMMAND_BITS.FSMCMD = Fapi_ClearStatus;
/* Execute the Clear Status command */
FLASH_CONTROL_REGISTER->FsmExecute.FSM_EXECUTE_BITS.FSMEXECUTE = 0x15U;
/* Write address to FADDR register */
FLASH_CONTROL_REGISTER->Faddr.u32Register = 0x00180000U;
//xxx FLASH_CONTROL_REGISTER->Faddr.u32Register = 0x0100U;
/* Placing byte at address 0x0102 */
oFwpWriteByteAccessor[2] = 0xA5;
/* Set command to "Program" */
FLASH_CONTROL_REGISTER->FsmCommand.FSM_COMMAND_BITS.FSMCMD = Fapi_ProgramData;
/* Execute the Program command */

/*
* Immediately after this step is executed the FMSTAT.CSTAT bit (any failure)
* goes high, as does the FMSTAT.PGV (write timeout?)
*/
FLASH_CONTROL_REGISTER->FsmExecute.FSM_EXECUTE_BITS.FSMEXECUTE = 0x15U;

/* re-lock FSM registers to prevent writing */
FLASH_CONTROL_REGISTER->FsmWrEna.u32Register = 0x2U;
}

Thanks.