Other Parts Discussed in Thread: TMS570LS1227, HALCOGEN
Hi,
In HTU Module of TMS570Ls1227, How many double control packets DCP there are?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS570LS1227, HALCOGEN
Hi,
In HTU Module of TMS570Ls1227, How many double control packets DCP there are?
Thanks
Enrico,
Thank you for using our e2e forum.
I've forwarded your question to our HTU expert.
Hello Enrico,
There are 8 Double Control Packets in HTU.
regards,
Charles
Hi Charles,
Thank very much for your fast response.
I'm using Halcogen 3.6.0 and I don't find any structure with 8 DCPs in reg_htu.h file.
Thanks
Hello Enrico,
Can you please take a look at the htu.h. You can find the DCP structure. Below is a snippet.
typedef volatile struct htuCP
{
unsigned IFADDRA; /** Initial main memory address Control Packet A */
unsigned IFADDRB; /** Initial main memory address Control Packet B */
unsigned IHADDRCT; /** Initial NHET address and control */
unsigned ITCOUNT; /** Initial transfer count */
} htuCP_t;
typedef volatile struct htuCPRamBase
{
htuCP_t DCP[8U];
} htuCPRAMBASE_t;
#define htuCPRAM ((htuCPRAMBASE_t *)0xFF4E0000U)
regards,
Charles
Hi Charles,
What Halcogen version do you use?
Halcogen version 3.6.0 and 3.8.0 doesn't generate htu.h file with DCP structure.
Enrico
Hello Enrico,
I just use 3.6.0 to generate the drivers for HTU. I'm able to find the DCP structures in reg_htu.h. Please see below. In my last reply I was looking at an existing project that I had before which has the DCP structure defined in htu.h. Something might have change since then.
typedef volatile struct htudcp
{
uint32 IFADDRA;
uint32 IFADDRB;
uint32 IHADDRCT;
uint32 ITCOUNT;
} htudcp_t;
typedef volatile struct htucdcp
{
uint32 CFADDRA;
uint32 CFADDRB;
uint32 CFCOUNT;
uint32 rsvd4;
} htucdcp_t;
#define htuREG1 ((htuBASE_t *)0xFFF7A400U)
#define htuREG2 ((htuBASE_t *)0xFFF7A500U)
#define htuDCP1 ((htudcp_t *)0xFF4E0000U)
#define htuDCP2 ((htudcp_t *)0xFF4C0000U)
#define htuCDCP1 ((htucdcp_t *)0xFF4E0100U)
#define htuCDCP2 ((htucdcp_t *)0xFF4C0100U)
regards,
Charles