Other Parts Discussed in Thread: TM4C123GH6PM
Hi guys!
I am doing a PWM project on my TM4C123GH6PM evaluation board.
PWM output 0 and 1 through PWM_GEN_0 are working fine. Pin PD0 and PD1 on J3.
Need some help on getting PWM output 2 and 3. It should go through PWM_GEN_1 (datasheet) and supposedly either pin PE4 and PE5 on J1, or pin PA6 and PA7 on J1.
This is my code so far:
Void pwmInit(Void)
{
// PWM settings
PWM_FREQUENCY = 400;
ui8Adjust = 440;
SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_OSC_MAIN|SYSCTL_XTAL_16MHZ);
SysCtlPWMClockSet(SYSCTL_PWMDIV_64);
SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM1);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
// PWM PD0, motor A
GPIOPinTypePWM(GPIO_PORTD_BASE, GPIO_PIN_0);
GPIOPinConfigure(GPIO_PD0_M1PWM0);
// PWM PD1, motor B
GPIOPinTypePWM(GPIO_PORTD_BASE, GPIO_PIN_1);
GPIOPinConfigure(GPIO_PD1_M1PWM1);
// PWM PD1, motor C
GPIOPinTypePWM(GPIO_PORTD_BASE, GPIO_PIN_2);
GPIOPinConfigure(GPIO_PE4_M1PWM2);
// PWM PD1, motor C
GPIOPinTypePWM(GPIO_PORTD_BASE, GPIO_PIN_3);
GPIOPinConfigure(GPIO_PE5_M1PWM3);
// For pushbuttons
HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
HWREG(GPIO_PORTF_BASE + GPIO_O_CR) |= 0x01;
HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = 0;
GPIODirModeSet(GPIO_PORTF_BASE, GPIO_PIN_4|GPIO_PIN_1, GPIO_DIR_MODE_IN);
GPIOPadConfigSet(GPIO_PORTF_BASE, GPIO_PIN_4|GPIO_PIN_1, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPU);
// PWM clk and frequency
ui32PWMClock = SysCtlClockGet() / 64;
ui32Load = (ui32PWMClock / PWM_FREQUENCY) - 1;
PWMGenConfigure(PWM1_BASE, PWM_GEN_0, PWM_GEN_MODE_DOWN);
PWMGenPeriodSet(PWM1_BASE, PWM_GEN_0, ui32Load);
PWMGenConfigure(PWM1_BASE, PWM_GEN_1, PWM_GEN_MODE_DOWN);
PWMGenPeriodSet(PWM1_BASE, PWM_GEN_1, ui32Load);
// PWM 0 and 1
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_0, (ui8Adjust * ui32Load) / 1000);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_1, (ui8Adjust * ui32Load) / 1000);
PWMOutputState(PWM1_BASE, PWM_OUT_0_BIT, true);
PWMOutputState(PWM1_BASE, PWM_OUT_1_BIT, true);
// PWM 2 and 3
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_2, (ui8Adjust * ui32Load) / 1000);
PWMPulseWidthSet(PWM1_BASE, PWM_OUT_3, (ui8Adjust * ui32Load) / 1000);
PWMOutputState(PWM1_BASE, PWM_OUT_2_BIT, true);
PWMOutputState(PWM1_BASE, PWM_OUT_3_BIT, true);
PWMGenEnable(PWM1_BASE, PWM_GEN_0);
PWMGenEnable(PWM1_BASE, PWM_GEN_1);
}
Anybody have some inputs for me? Do I maby have my PWM1_BASE mixed up?