I am having trouble getting the 7970ABP RFID module to work with my Tiva C Series Launchpad TM4C123GXL.
The product information states: Compatible with the TIVA C Series LaunchPad.
I am connected to the Launchpad in debug mode and my COM port is "Stellaris Virtual Serial Port (COM3)". When I attached the 7970 with pin 1 to 3.3V and pin 20 to ground, the Launchpad will not power on. The boards are right on top of each other with this pin alignment, as opposed to offset.