This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI File system example



I am using example provided by TI located in:

C:\ti\TivaWare_C_Series-2.0.1.11577\examples\boards\dk-tm4c129x\sd_card

1. file "ff_conf.h" contains "#define _CODE_PAGE 932". What is its use. Due to this cc932.c gets included & its has large constant data in memory. Although I have enough memory but can I remove it.  Almost 30K of constant data.

I want to use long file names along with it.

2.  I had make a file "file.txt", successfully crated it & read data & them I can read that file in PC also.

   But on creating file "data.xlsx" , file gets created successfully in MCU, but when I transfer that file in PC, windows don't open that file & return error

"Excel cannot open the file because file format or file extension is not valid. verify that file not corrupted and that file extension matches the format of file".

Obviously there could be different format for writing excel. But I don't what it is. I want to write data in different cells.

    for(bw = 0 ; bw < 512 ; bw++)
    {
        my_buf[bw] = 0x31;        /* write 1 in ascii */
    }
    
/* mount drive */    
	x = f_mount(0 , &FatFs);		/* Give a work area to the default drive */

/* open/create a text file */
    x = f_open(&Fil, "/file.txt", FA_WRITE | FA_OPEN_ALWAYS);
    x = f_lseek(&Fil, f_size(&Fil));  
    x = f_write(&Fil, &my_buf[0], 512, &bw);	/* Write data to the file */    
    x = f_close(&Fil);								/* Close the file */
      

/* open/create a excel file */    
    x = f_open(&Fil, "/my_file.xlsx", FA_WRITE | FA_OPEN_ALWAYS);
    x = f_lseek(&Fil, f_size(&Fil));  
    x = f_write(&Fil, &my_buf[0], 512, &bw);	/* Write data to the file */
    x = f_close(&Fil);								/* Close the file */

  • Hi,

    Whether you like it or not, to have a .xlsx file, you must follow the rules for that kind of file, otherwise reading it on PC gives you the shown error. Here you have an example of internal structure of such file. 

    If this is too complicated for your application, you may try to make a comma separated value (.csv) file instead.

    Petrei