Other Parts Discussed in Thread: HALCOGEN, TMS570LS0432
Hello Support,
I see that pbistSelfCheck() in HALCOGEN 3.08.01 is not using the following any more due to PBIST ERRATA #4
/* Algorithm code is loaded from ROM */
pbistREG->ROM = 0x3U;
Instead it is using some hidden command sequence.
But for pbistRun(), I see that it is using the same old method as mentioned above.
Can you please explain why old method will not work for pbistSelfCheck() but it will still work for pbistRun()?
Or, I am missing something.
Any better explanations related to the PBIST ERRATA #4 as performed within HALCOGEN 3.08.01 will help me a lot.
Is it that PBIST ERRATA #4 occurs for only FAIL Test case of FSRF0 and FSRF1 bits [Stuck at ZERO test]?
Thank you.
Regards
Pashan