Dear Stellaris Champions,
One of my ctm want to update FW via Ethenet using LM flash programmer. When they use it, they need to input both IP and MAC address. Ctm think it is not convenient for them to find and input MAC address every time.
So my question is:
1) Why we need to input MAC address when use this function?
2) Can we upgrade FW by only input IP address without MAC address
Thanks.
Best Regards,
Holly