Other Parts Discussed in Thread: TM4C129XKCZAD, TM4C1230C3PM
Hi,
I need to know what is the input ESD protection of analogue pins of the TM4C129XKCZAD? http://www.ti.com/lit/ds/symlink/tm4c129xkczad.pdf
Form the description and the figure 32-29 the ESD clamp looks like the one of the Hibernate Wake pin. But the description in chapter 32.14.1 says: ‘All pins except the hibernate wake pin are protected like shown for the non-power pins.’ But these pins have a clamp diode to supply voltage, which is explicitly not present at the ADC.
How are the ADC pins protected? It says there is a 5V ESD clamp. Does it really become active not before voltages rise higher than 5V? The Fail-Safe pin description of the TM4C123x would give me all this information. http://www.ti.com/lit/ds/symlink/tm4c1230c3pm.pdf.
I also read this: http://www.ti.com/lit/an/spma056/spma056.pdf, but it did not answer my questions.