Other Parts Discussed in Thread: HALCOGEN
I am programming the TI hercules launchpad spi feature and am unable to overcome the following highlighted errors:
Below is the content from output window
'Invoking: ARM Linker'
"C:/ti/ccsv5/tools/compiler/arm_5.1.1/bin/armcl" -mv7R4 --code_state=32 --abi=eabi -me -g --diag_warning=225 --display_error_number --diag_wrap=off --enum_type=packed -z -m"freya.map" --heap_size=0x800 --stack_size=0x800 -i"C:/ti/ccsv5/tools/compiler/arm_5.1.1/lib" -i"C:/ti/ccsv5/tools/compiler/arm_5.1.1/include" --reread_libs --warn_sections --display_error_number --diag_wrap=off --xml_link_info="freya_linkInfo.xml" --rom_model -o "freya.out" "./source/system.obj" "./source/sys_vim.obj" "./source/sys_startup.obj" "./source/sys_selftest.obj" "./source/sys_pmu.obj" "./source/sys_phantom.obj" "./source/sys_pcr.obj" "./source/sys_mpu.obj" "./source/sys_intvecs.obj" "./source/sys_core.obj" "./source/sci.obj" "./source/pinmux.obj" "./source/notification.obj" "./source/esm.obj" "./source/dabort.obj" "./main.obj" "../RM42L432FlashLnk.cmd" "../source/sys_link.cmd" -l"libc.a"
<Linking>
"../source/sys_link.cmd", line 24: error #10263: VECTORS memory range has
already been specified
"../source/sys_link.cmd", line 24: error #10264: VECTORS memory range overlaps
existing memory range VECTORS
"../source/sys_link.cmd", line 25: error #10263: FLASH0 memory range has
already been specified
"../source/sys_link.cmd", line 25: error #10264: FLASH0 memory range overlaps
existing memory range FLASH0
"../source/sys_link.cmd", line 26: error #10263: STACKS memory range has
already been specified
"../source/sys_link.cmd", line 26: error #10264: STACKS memory range overlaps
existing memory range STACKS
"../source/sys_link.cmd", line 26: error #10264: STACKS memory range overlaps
existing memory range RAM
"../source/sys_link.cmd", line 27: error #10263: RAM memory range has already
been specified
"../source/sys_link.cmd", line 27: error #10264: RAM memory range overlaps
existing memory range RAM
warning #10366-D: automatic library build: using library "C:\ti\ccsv5\tools\compiler\arm_5.1.1\lib\rtsv7R4_A_le_eabi.lib" for the first time, so it must be built. This may take a few minutes.
0 [main] sh 10180 open_stackdumpfile: Dumping stack trace to sh.exe.stackdump
C:/Users/Anurag/AppData/Local/Temp/make13440-1.sh: line 1: 10180 Segmentation fault (core dumped) c:/ti/ccsv5/tools/compiler/arm_51~1.1/bin/armar -qa c:/users/anurag/appdata/local/temp/ti5ed1~1/rtsv7r4_a_le_eabi.lib *.obj
gmake.exe[1]: *** [library] Error 139
>> ERROR: mklib: gmake error during rtsv7R4_A_le_eabi.lib build
warning #10207-D: automatic RTS selection: resolving index library "libc.a" to "C:\ti\ccsv5\tools\compiler\arm_5.1.1\lib\rtsv7R4_A_le_eabi.lib", but "C:\ti\ccsv5\tools\compiler\arm_5.1.1\lib\rtsv7R4_A_le_eabi.lib" was not found
undefined first referenced
symbol in file
--------- ----------------
__TI_auto_init ./source/sys_startup.obj
__TI_decompress_none
__TI_decompress_rle24
__TI_zero_init
>> Compilation failure
__aeabi_d2uiz ./source/sci.obj
__aeabi_ddiv ./source/sci.obj
__aeabi_ui2d ./source/sci.obj
exit ./source/sys_startup.obj
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "freya.out" not built
gmake: *** [freya.out] Error 1