Other Parts Discussed in Thread: DRV8301
Hello,
I am in urgent need of help with this.
I have CCS v5, and I want to upload what software is running on the tms570 microcontroller into the CCS IDE.
Then once the code is in the IDE I want to recompile it and download it to the microcontroller.
I want to do this using the example that comes with the DRV8301 kit under the file directory:
"C:/ti/guicomposer/webapps/DRV8301_TMS570_BLDC" -or- any other examples would be fantastic.
I have been at this problem for a while now and I seem to be missing something.
I greatly appreciate any help that can be provided. Thank you,
Nate