Other Parts Discussed in Thread: TM4C123GH6PM, TM4C123GH6PGE
Dear TI community,
I’m willing to use the Tiva C microcontroller (TM4C123GH6PM) to read a USB keyboard, thus I need the microcontroller to operate as a host, I want it to send the read characters to the UART0.
The available example in TivaWare (USB_host_keyboard) is designed for TM4C123GH6PGE and it needs some modifications.
Can anyone help me with these modifications? or provide a working code?
Also I want to check the hardware, I built a dedicated hardware with a USB host connector (female Type A USB connector) similar to the one on our PCs, it has four pins only, I connected them to 5V, DM, DP and GND in pins 1 through 4 respectively.
Do I have to do any modifications in Hardware?
Thank you for the support.
Best regards,
Mina