Hello,
I am using the stellaris launchpad.When i load the program from the myLaunchpadBoard / lab4 than it is working correctly and it is for the timer0 based interrupt but i want to run it with timer1. so that in the whole program where timer0 is present i replace it with timer1 and i also change the interrupt function name but it is going to infinite loop.what the problem with it ?