Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Does STC Self Test as well as Stuck Bit Test for STC depends upon VIM INTREQ being active?

Hello Support,

If before STC Self Test [pass condition as well as fail condition (for STUCK Bit Test)] depends if VIM INTREQ is active for IRQ but Cortex-R4 core CPSR I-Bit is disabled?

Assume VIM RAM is unprogrammed or corrupt. By any chance during STC Self Test, CPSR I-Bit becomes ENABLED [IRQ Enabled] and VIM INTREQ being active, IRQ Vector is called.

Please confirrm what will happen if VIM INTREQ is active and VIM RAM Unprogrammed during STC Self Test, when user have disabled CPSR I-Bit [IRQ Disabled].

Thank you.
Regards
Pashan

  • Pashan,

    During STC Self Test, the CPUs (0 and 1) are in complete isolation from the rest of the system.
    Any VIM request (IRQ or FIQ) will be ignored during STC.
    When STC is done, and CPU resets, it is necessary to restore all CPU context. At that point, if CPSR_i is restored to 0 (IRQ enable) than the CPU will service the highest pending request on the VIM.