Other Parts Discussed in Thread: TM4C1233H6PZ
Hi,
I'm working with a TM4C1233H6PZ on a board that I developed. I'm seeing an issue where I2C0SDA line on PB3 is held low after reset/power up.
I do have 1.62k pull ups to 3.3VDC on both the SDA and SCL lines.
I have found that it requires ~60mA at 3.3VDC to pull the SDA line high. If I write to the I2C bus while I have it pulled hard high, it fails arbitration, but the ~60mA drain disappears and I can remove the hard pull up. After this point the bus works properly until the Tiva is reset.
The following is my configuration code and my writing code. This code works properly with the four other I2C busses I am using on the chip.
if (!ROM_SysCtlPeripheralReady (SYSCTL_PERIPH_GPIOB))
{
DEBUG_PRINT2("GPIO B peripheral not enabled...\n");
SysCtlPeripheralEnable (SYSCTL_PERIPH_GPIOB);
while (!SysCtlPeripheralReady (SYSCTL_PERIPH_GPIOB)) {
DEBUG_PRINT2("Waiting\n");
}
}
DEBUG_PRINT2("Enabling I2C Bus 0...\n");
ROM_GPIOPinTypeI2C (GPIO_PORTB_BASE, GPIO_PIN_3);
GPIOPinTypeI2CSCL (GPIO_PORTB_BASE, GPIO_PIN_2);
GPIOPinConfigure (GPIO_PB2_I2C0SCL);
GPIOPinConfigure (GPIO_PB3_I2C0SDA);
SysCtlPeripheralEnable (SYSCTL_PERIPH_I2C0);
I2CMasterInitExpClk(I2C0_BASE, SysCtlClockGet(), true);
I2CMasterEnable(I2C0_BASE);
break;
void i2cWrite(uint32_t busNumber)
{
uint32_t I2CBaseValue = 0;
char i2cBusString[0];
uint32_t count = 0;
switch (busNumber)
{
case 0:
{
I2CBaseValue = I2C0_BASE;
strcpy(i2cBusString, "0");
break;
}
case 1:
{
I2CBaseValue = I2C1_BASE;
strcpy(i2cBusString, "1");
break;
}
case 2:
{
I2CBaseValue = I2C2_BASE;
strcpy(i2cBusString, "2");
break;
}
case 3:
{
I2CBaseValue = I2C3_BASE;
strcpy(i2cBusString, "3");
break;
}
case 4:
{
//Bus Not Used.
return;
}
case 5:
{
I2CBaseValue = I2C5_BASE;
strcpy(i2cBusString, "5");
break;
}
}
count = 0;
UARTprintf("I2C Port ");
UARTprintf(i2cBusString);
UARTprintf("\n");
ROM_I2CMasterSlaveAddrSet(I2CBaseValue, strtol(inputCommand.address, NULL, 16), false);
ROM_I2CMasterDataPut(I2CBaseValue, inputCommand.data[count]);
if(dataSize > 1)
{
DEBUG_PRINT4("DATASIZE BURST %d\n", dataSize);
ROM_I2CMasterControl(I2CBaseValue, I2C_MASTER_CMD_BURST_SEND_START);
count++;
while(count < dataSize)
{
while(ROM_I2CMasterBusy(I2CBaseValue))
{
DEBUG_PRINT4("I2C3 Master Busy\n");
}
DEBUG_PRINT3("Current Data Byte: %u\n", count);
ROM_I2CMasterDataPut(I2CBaseValue, inputCommand.data[count]);
ROM_I2CMasterControl(I2CBaseValue, I2C_MASTER_CMD_BURST_SEND_CONT);
count++;
}
ROM_I2CMasterControl(I2CBaseValue, I2C_MASTER_CMD_BURST_SEND_STOP);
}
else
{
if(strcmp(inputCommand.type, "I2CS") == 0)
{
ROM_I2CMasterControl(I2CBaseValue, I2C_MASTER_CMD_BURST_SEND_START);
}
else
{
ROM_I2CMasterControl(I2CBaseValue, I2C_MASTER_CMD_SINGLE_SEND);
}
}
switch (I2CMasterErr(I2CBaseValue))
{
case I2C_MASTER_ERR_NONE:
{
UARTprintf("No I2C Error\n");
break;
}
case I2C_MASTER_ERR_ADDR_ACK:
{
UARTprintf("I2C Address Ack Error\n");
break;
}
case I2C_MASTER_ERR_DATA_ACK:
{
UARTprintf("I2C Data Ack Error\n");
break;
}
case I2C_MASTER_ERR_ARB_LOST:
{
UARTprintf("I2C Arbitration Lost\n");
break;
}
}
return;
}
Any suggestions or recommendations will be gladly accepted.
Thanks,
Jed